Eaton Customer Success Stories from around the World
Customers around the world depend on UPS, services and power quality solutions from Eaton to keep their applications up and running without interruption. Read more about how customers rely on Eaton every day in our latest success stories.
All Success Stories
Title | Date |
---|---|
Eaton and Amdocs collaborate to create an efficient data center “The outstanding efforts of Eaton and Carter Sullivan made it possible to complete the Amdocs data center on schedule and on budget” Learn more... |
2/4/2018 |
CityServiceValcon with Nutanix Hyperconverged Eaton`s hyperconverged infrastructure solution allows CityServiceValcon to have continuous uptime in their virtualized environment Learn more... |
8/23/2017 |
Eaton provides Webaxys’ new eco-designed data center with a complete energy storage and management system Webaxys is a hosting company and telecom operator located in Normandy, France. Since its inception in 2003, the company has pursued a strategy of innovation based on strong values of social engagement and respect for the environment. Learn more... |
11/20/2016 |
Eaton enables always-on operations for 100 percent renewable power data center Verne Global owns and operates a 44-acre data center campus in Keflavik, Iceland. The strategic location provides availability to the world’s two largest data center markets, Europe and North America, while also addressing some of the most critical challenges facing today’s data center landscape. Learn more... |
10/13/2016 |
SAMSØ ferry power system maintains ecological requirements of one of the wonders of the world Flexible, intelligent and safe power conversion UPS system meets both the environmental and power needs for transport between island and the mainland Learn more... |
4/25/2016 |
Eaton gives energy efficiency a boost in Meilahti Tower Hospital Eaton’s reliable UPS devices secure power for the hospital’s mission-critical applications whilst meeting the demand for high energy efficiency, exceeding the set goal of 1-hour+ power continuity. Learn more... |
4/18/2016 |
Eaton гарантирует бесперебойное электропитание для компании Total Cloud Компания Total Cloud выбрала решения Eaton по управлению электропитанием, и это позволяет её центру обработки данных работать без перебоев. Learn more... |
4/13/2016 |
Eaton provides BlueFjords data center with power that’s efficient and expandable The utility power to the BlueFjords data center can be expected to be reliable for the majority of the time thanks to its proximity to the power node. However, power protection is still vital to ensure that the operation of the data center is never disrupted by power problems such as transients, power surges and voltage perturbations. Learn more... |
4/7/2016 |
Teraco tackles load shedding, efficiency and management issues with Power Xpert 9395 UPS Teraco was formed to take advantage of large scale deregulation of the telecommunications sector in South Africa, and has grown at an exponential rate, validating their business model; a large proportion of the large enterprises in South Africa rely on Teraco for interconnection services. Learn more... |
9/7/2015 |
Eaton Prevents Milk Malfunction The Roshen milk processing plant in Vinnitsa experiences, on average, three to four mains electricity supply failures each quarter. When these failures occur, the effects on the dryers used to convert liquid milk into dehydrated milk powder are costly and disruptive. Learn more... |
6/23/2015 |
E4 Computer Engineering SpA - ICT services provider Eaton cooperates with Italian E4 to design a totally integrated, scalable and fault tolerant E4 VSTONE converged infrastructure solution for private clouds. Learn more... |
4/30/2015 |
DPC BSTelecom works with Eaton to bring energy efficiency to in demand Russian data Eaton UPS helped to create a reliable, efficient, trouble-free and cost-effective data center uninterruptible power supply system for BSTelecom. Learn more... |
4/21/2015 |
Eaton Ensures Reliable and Uninterrupted Operation of Laboratory Equipment for Swiss Pharmaceutical The Eaton 93PM UPS ensures long-term, reliable and uninterrupted operation of Roche’s laboratory equipment even under heavy load. Learn more... |
4/21/2015 |
Eaton Powers the Bolshoi Theatre The Bolshoi Theatre and its warehouse now have a robust power supply system based on Eaton UPS technology. Learn more... |
4/21/2015 |
Eaton`s Data Centre Solutions Provide Cost Savings for Eastbourne College Eaton’s comprehensive data centre offering has provided Eastbourne College with an integrated and highly efficient infrastructure for its new data centre at half the cost of the solutions offered by turnkey suppliers. Learn more... |
4/7/2015 |
«Донбасс Арена» готова к Евро-2012 Недавно открывшаяся «Донбасс Арена», вместимостью более 50 000 зрителей, является первым футбольным стадионом в Восточной Европе, спроектированным и построенным согласно стандартам элитной категории УЕФА. Learn more... |
6/29/2014 |
Cinesa – Cinema operator Eaton 5PX UPS and Intelligent Power software protects virtualised IT systems at 46 locations of Cinesa, one of the region´s leading cinema operators. Learn more... |
5/15/2014 |
Illiad Datacenter В центре DC2 компании Iliad используется пять модулей ИБП Eaton 9395 550 кВА с совокупной мощностью 2500 кВт. Learn more... |
5/6/2014 |
Sentrum Надежность, гибкость и эффективность: система бесперебойного питания для Sentrum Learn more... |
5/6/2014 |
Дата-центр: представить инновации, достойные Facebook. Когда Facebook достиг уровня одного из наиболее энергоэффективных операторов центров обработки данных в мире, мы переняли их смелые взгляды. Центры обработки данных потребляют колоссальное количество энергии - 1,7%-2,2% от всей электроэнергии, потребляемой в США. Learn more... |
5/6/2014 |
KUVAG – Insulator manufacturer KUVAG’s site in Neumarkt am Hausruck is known for its two specialist products—medium and high-voltage insulators—far beyond the Austrian border. Learn more... |
4/28/2014 |
MKW Holding – Plastic manufacturer To give a summary of its key economic figures, MKW is spread across four sites, operates four manufacturing facilities and generates an annual turnover of 50 million euros. Learn more... |
4/28/2014 |
Seidel Elektronik – Manufacturing services Seidel Elektronik is a popular contract manufacturer, whose production lines rarely stand idle. Learn more... |
4/28/2014 |
Senoplast – Plastic manufacturer While many others were still experimenting with harder materials, in 1956 Senoplast founder Wilhelm Klepsch discovered plastic as a promising material for his business plan. Learn more... |
4/28/2014 |
Econocom – ICT services provider Econocom is collaborating with Eaton on the development of viCUBE in relation to racks, intelligent ePDUs, UPSs as well as Eaton´s power management software called Intelligent Power™. Learn more... |
4/1/2014 |
Virtus – Colocation provider Virtus Data Centres provides modern and flexible colocation space to support London’s financial, media, cloud and digital businesses. The company’s data centres are designed with both environmental efficiency and high connectivity in mind. Learn more... |
3/9/2014 |
Bakhresa – Milk production plant Eaton UPS equipment with doubleconversion technology provides the best available protection against all types of power quality problems and offers class-leading efficiencies of up to 99 percent Learn more... |
12/5/2013 |
ServeisWeb – Internet service provider The two new UPSs were installed with no downtime and, alongside the existing units, provide continuous, conditioned, reliable electricity enabling ServeisWeb’s level of service to be maintained. Learn more... |
9/24/2013 |
NURTS Bulgaria – Radio and television broadcaster NURTS Bulgaria AD identified that it needed to modernise its backup power supplies to ensure its network is thoroughly protected against power outages and operating at the highest level of efficiency possible. With an efficiency rating of over 95 per cent, Eaton 9130 rack mount UPSs were selected for their energy saving potential. Learn more... |
9/3/2013 |
Granite Networks – Colocation provider Data center firm achieves 100% uptime with 9395 UPS. Learn more... |
8/17/2013 |
IDentiphoto – ID technology systems integrator Firm quick to ID value, efficiency in Eaton 5P. Learn more... |
8/17/2013 |
Kortek Solutions – ICT services provider Eaton efficiency, software are stands outs for IT firm. Learn more... |
8/17/2013 |
Automatia – Cash distributor "Eaton UPSs ensure safe, reliable power to all 1,640 Otto cash machines in Finland and help achieve a utilisation rate of 98.5 per cent. The UPS`s effective remote control, smart energy management and easy maintenance enable Automatia to cut operational and service costs." Learn more... |
7/18/2013 |
Grand Cinema Digiplex – Cinema operator Eaton`s UPS technology allows visitors to the cinema continuous enjoyment of the film experience while only taking up minimal space. Learn more... |
7/18/2013 |
Tissat – ICT services provider Eaton`s 9395 UPSs are helping the award winning Walhalla data centre achieve 99.995 per cent availability Learn more... |
7/18/2013 |
STX Finland – MS Viking Grace cruise ferry The total capacity of the UPS systems aboard the new vessel was more than 200 kVA. All of the UPSs chosen for this project are versions which have been optimised for marine applications and which have already gained a strong reputation for performance and reliability aboard sea-going vessels in every part of the world. Learn more... |
6/11/2013 |
Markley – Colocation provider Power Xpert 9395 units deliver high reliability, efficiency at mission-critical data center facility. Learn more... |
5/1/2013 |
Williams – Energy infrastructure provider Power Xpert 9395 delivers high reliability, efficiency for natural gas transporter. Learn more... |
5/1/2013 |
Iliad Group – Data centre operator During the modernisation of its 5,000 m2 DC2 site in Vitry, Paris, Iliad Datacenter needed a reliable UPS installation that would enable the company to increase its energy efficiency without compromising on service quality. Learn more... |
8/17/2012 |
Royal Institute of Technology – Technical University Uninterrupted research and unprecedented energy saving at KTH Learn more... |
6/6/2012 |
Previder – ICT services provider Dutch ICT service provider Previder offers spacious, ultra-modern and energy-efficient data centres that meet the needs of today and tomorrow. At their new data centre in Hengelo, everything concerning power supply and security is done twice or often even three times over. To ensure uninterrupted, 24/7 availability, the company chose Eaton as their electrical supply system provider. Learn more... |
9/28/2011 |
Stadtwerke Flensburg – Utility services provider German utility company Stadtwerke Flensburg is constantly developing new areas of activity. In 2010 they set up a modern, energy-efficient data centre large enough to not only host the servers for the company’s own applications, but also to allow data centre space to be leased out. Learn more... |
5/16/2011 |
Skåne University – Hospital Eaton´s power quality solutions contribute to maintaining the Skane University hospital´s vital functions in Malmö, Sweden. Learn more... |
3/30/2011 |
Royal Caribbean – Allure of the Seas cruise ship Eaton delivered over 20 doubleconversion, online marine UPSs to the ship. On board the ship is the first ever marine application of Eaton’s Energy Saver System (ESS) technology, which enables the UPS devices to reach an industry-leading efficiency level of 99 per cent. Learn more... |
3/21/2011 |
Global Switch – Colocation provider Leading data centres need leading power protection. Learn more... |
2/7/2011 |
Bahnhof – Internet service provider The centre relies on Eaton’s UPS protection to provide rock-solid network operations and colocation services. Learn more... |
8/5/2010 |
IBM – Portable modular data center Eaton has been chosen as one of the power management partners for IBM’s Portable Modular Data Center (PMDC) solution. Learn more... |
8/5/2010 |
North Estonia Medical Centre – Hospital The North Estonia Medical Centre chose Eaton UPSs to protect its patients’ lives. Learn more... |
8/5/2010 |
Royal Caribbean – Oasis of the Seas cruise ship Eaton supplied more than 20 double-conversion online UPSs for this giant of the seas. Learn more... |
1/20/2010 |
Citi – Financial services provider Global financial services company Citi chose Eaton 9390 UPSs to protect its Barcelona Sales and Services Centre from potentially damaging power losses. Learn more... |
1/14/2010 |
Список

- ИБП для компьютеров и рабочих станций
- Eaton Protection Station (500-800BA)
- Eaton 3S (550-700 ВА)
- Eaton Ellipse ECO (500-1600BA)
- Eaton 5E (500-2000BA)
- Eaton 5S (550 - 1500ВA)
- Eaton Ellipse PRO (650-1600 ВA)
- ИБП для сетевого и серверного оборудования
- Eaton 5SC (500 - 3000ВA)
- Eaton 5P (650 – 1550Ва)
- Eaton 5PX (1500-3000 BA)
- E Series DX (1-20 кВА)
- Eaton EX (700 - 1500 BA)
- Eaton 9SX (700-3000 ВA) – замена 9130
- Eaton 9SX (5-11 кВА) – замена 9130
- Eaton 9PX (1-3 кВА)
- Eaton 9PX (5-22 кВА)
- Eaton 9E (6-20 кВА)
- Eaton 9155 (8-30 KBA)
- ИБП с двойным преобразованием для ЦОД и ответственной электроники
- BladeUPS (12-60 kW)
- ИБП Eaton 91PS и 93PS (8-30 / 40 кВт)
- Eaton 93PM (30-500 kВА)
- Eaton 93E (15 - 200 кВА)
- Power Xpert 9395P (250-1200 kBA)
- Системы постоянного тока (DC)
Latest successes
SAMSØ ferry power system maintains ecological requirements of one of the wonders of the world Eaton and Amdocs collaborate to create an efficient data center |
Дополнительная информация
|
Пресс-центр |