Eaton Customer Success Stories from around the World

Customers around the world depend on UPS, services and power quality solutions from Eaton to keep their applications up and running without interruption. Read more about how customers rely on Eaton every day in our latest success stories.

Filter by...

All Success Stories

Title Date
Eaton UPS in CE Colo data center environment
In 2015, CE Colo started to address the technological renovation of the existing UPS system. Two independent manufacturers capable of delivering technologies that are required for the challenging data center environment were selected. The reconstruction of the existing functional system required the implementation of a new solution to prevent the renovation from having any impact on the 24/7 operation and the customers.
En savoir plus ...
4/15/2019
Landsvirkjun works with Eaton to bring reliable and environmental reserve
Landsvirkjun, the National Power Company of Iceland, is Iceland’s largest electricity generator and one of the ten largest producers of renewable energy in Europe. Landsvirkjun operates 18 power plants in Iceland, and they also operate two windmills as a research and development test site.
En savoir plus ...
4/8/2019
New UPS and supercapacitor technology at the heart of hospital
The Pirkanmaa Hospital District (PSHP) worked with Eaton to install modern UPSs with supercapacitor technology to ensure uninterruptible operation of hospital imaging devices.
En savoir plus ...
2/25/2019
Eaton and Amdocs collaborate to create an efficient data center
“The outstanding efforts of Eaton and Carter Sullivan made it possible to complete the Amdocs data center on schedule and on budget”
En savoir plus ...
2/4/2018
CityServiceValcon with Nutanix Hyperconverged
Eaton`s hyperconverged infrastructure solution allows CityServiceValcon to have continuous uptime in their virtualized environment
En savoir plus ...
8/23/2017
Eaton valide chez Webaxys une solution de stockage d’énergie et gestion de datacenter éco-conçu ?
La société Webaxys, hébergeur et opérateur télécom implanté en Normandie poursuit, depuis sa création en 2003, une stratégie d’innovation basée sur des valeurs fortes d’engagement sociétal et de respect de l’environnement.
En savoir plus ...
11/21/2016
Eaton provides Webaxys’ new eco-designed data center with a complete energy storage and management system

Webaxys is a hosting company and telecom operator located in Normandy, France. Since its inception in 2003, the company has pursued a strategy of innovation based on strong values of social engagement and respect for the environment.


En savoir plus ...
11/20/2016
Eaton enables always-on operations for 100 percent renewable power data center
Verne Global owns and operates a 44-acre data center campus in Keflavik, Iceland. The strategic location provides availability to the world’s two largest data center markets, Europe and North America, while also addressing some of the most critical challenges facing today’s data center landscape.
En savoir plus ...
10/13/2016
SAMSØ ferry power system maintains ecological requirements of one of the wonders of the world
Flexible, intelligent and safe power conversion UPS system meets both the environmental and power needs for transport between island and the mainland
En savoir plus ...
4/25/2016
Eaton donne un coup de boost à l’efficacité énergétique de l’hôpital Meilahti Tower.
La fiabilité des onduleurs Eaton permet de sécuriser les applications critiques de l’hôpital tout en répondant à la demande d’un rendement élevé et dépassant l’objectif fixé d’une heure d’autonomie.
En savoir plus ...
4/18/2016
Eaton fourni une énergie efficace et évolutive au Datacenter BlueFjords
La puissance énergétique du Datacenter BlueFjords peut être vu comme fiable la plupart du temps grâce à sa proximité avec la source. Cependant, la protection électrique est vitale afin de s’assurer que les opérations du Datacenter ne soient jamais perturbées par des problèmes d’alimentation électrique tels que les régimes transitoires, la foudre et les surtensions.
En savoir plus ...
4/7/2016
Eaton Garantit l’Activité sans Interruption du Data Center Total Cloud
Total Cloud est une société qui emploie huit personnes et dont le domaine d’activité est basé sur la vie de la donnée informatique, c’est-à-dire le stockage, la sauvegarde et l’archivage pour ses principales fonctions.
En savoir plus ...
2/16/2016
Teracao a répondu aux problèmes de partage des charges, d’efficacité et de gestion avec l’onduleur P
Teraco a été créé pour tirer avantage de la grande déréglementation du secteur des télécommunications en Afrique du Sud, grandissant à une croissance exponentielle, confirmant ainsi son business modèle. Une majorité de grandes entreprises en Afrique du Sud font confiance à Teraco pour les services d’interconnexion.
En savoir plus ...
9/7/2015
Eaton prévient des dysfonctionnement du lait
L’usine Roshen de transformation du lait basée à Vinnitsa, subissait en moyenne 3 à 4 grosse coupures de courant chaque trimestre. Durant ces coupures, les effets  sur les séchoirs utilisés pour convertir le lait liquide en poudre de lait déshydraté étaient coûteux et très perturbateurs.
En savoir plus ...
6/23/2015
Cinesa – l’exploitant cinématographique
Les onduleurs Eaton 5PX et le logiciel de gestion d’énergie associé Intelligent Power protègent 46 sites virtualisés de Cinesa, l’un des exploitants cinématographiques leader en Europe.
En savoir plus ...
5/31/2015
Partenariat Eaton & E4, société d’ingénierie informatique – Fournisseur d’accès
Eaton coopère avec l’italien E4 pour concevoir l’infrastructure convergée E4 VSTONE pour cloud privés, totalement intégrée, évolutive et tolérante aux pannes.
En savoir plus ...
4/30/2015
DPC BSTelecom works with Eaton to bring energy efficiency to in demand Russian data
Eaton UPS helped to create a reliable, efficient, trouble-free and cost-effective data center uninterruptible power supply system for BSTelecom.
En savoir plus ...
4/21/2015
Eaton Ensures Reliable and Uninterrupted Operation of Laboratory Equipment for Swiss Pharmaceutical
The Eaton 93PM UPS ensures long-term, reliable and uninterrupted operation of Roche’s laboratory equipment even under heavy load.
En savoir plus ...
4/21/2015
Eaton Powers the Bolshoi Theatre
The Bolshoi Theatre and its warehouse now have a robust power supply system based on Eaton UPS technology.
En savoir plus ...
4/21/2015
Eaton`s Data Centre Solutions Provide Cost Savings for Eastbourne College

Eaton’s comprehensive data centre offering has provided Eastbourne College with an integrated and highly efficient infrastructure for its new data centre at half the cost of the solutions offered by turnkey suppliers.


En savoir plus ...
4/7/2015
KUVAG – Insulator manufacturer
KUVAG’s site in Neumarkt am Hausruck is known for its two specialist products—medium and high-voltage insulators—far beyond the Austrian border.
En savoir plus ...
4/28/2014
MKW Holding – Plastic manufacturer
To give a summary of its key economic figures, MKW is spread across four sites, operates four manufacturing facilities and generates an annual turnover of 50 million euros.
En savoir plus ...
4/28/2014
Seidel Elektronik – Manufacturing services
Seidel Elektronik is a popular contract manufacturer, whose production lines rarely stand idle.
En savoir plus ...
4/28/2014
Senoplast – Plastic manufacturer
While many others were still experimenting with harder materials, in 1956 Senoplast founder Wilhelm Klepsch discovered plastic as a promising material for his business plan.
En savoir plus ...
4/28/2014
Econocom – ICT services provider
Econocom is collaborating with Eaton on the development of viCUBE in relation to racks, intelligent ePDUs, UPSs as well as Eaton´s power management software called Intelligent Power™.
En savoir plus ...
4/1/2014
Virtus – Colocation provider
Virtus Data Centres provides modern and flexible colocation space to support London’s financial, media, cloud and digital businesses. The company’s data centres are designed with both environmental efficiency and high connectivity in mind.
En savoir plus ...
3/9/2014
Facebook – Social networking company
Facebook leveraged the Power Xpert 9395 to help take its Power Usage Effectiveness (PUE) rating to well below the industry average.
En savoir plus ...
2/3/2014
Bakhresa – Milk production plant
Eaton UPS equipment with doubleconversion technology provides the best available protection against all types of power quality problems and offers class-leading efficiencies of up to 99 percent
En savoir plus ...
12/5/2013
ServeisWeb – Internet service provider
The two new UPSs were installed with no downtime and, alongside the existing units, provide continuous, conditioned, reliable electricity enabling ServeisWeb’s level of service to be maintained.
En savoir plus ...
9/24/2013
NURTS Bulgaria – Radio and television broadcaster
NURTS Bulgaria AD identified that it needed to modernise its backup power supplies to ensure its network is thoroughly protected against power outages and operating at the highest level of efficiency possible. With an efficiency rating of over 95 per cent, Eaton 9130 rack mount UPSs were selected for their energy saving potential.
En savoir plus ...
9/3/2013
Granite Networks – Colocation provider
Data center firm achieves 100% uptime with 9395 UPS.
En savoir plus ...
8/17/2013
IDentiphoto – ID technology systems integrator
Firm quick to ID value, efficiency in Eaton 5P.
En savoir plus ...
8/17/2013
Kortek Solutions
Efficacité Eaton, les logiciels sont des stands out pour la firme informatique.
En savoir plus ...
8/17/2013
Automatia – Cash distributor

"Eaton UPSs ensure safe, reliable power to all 1,640 Otto cash machines in Finland and help achieve a utilisation rate of 98.5 per cent. The UPS`s effective remote control, smart energy management and easy maintenance enable Automatia to cut operational and service costs."


En savoir plus ...
7/18/2013
Grand Cinema Digiplex – Cinema operator
Eaton`s UPS technology allows visitors to the cinema continuous enjoyment of the film experience while only taking up minimal space.
En savoir plus ...
7/18/2013
Tissat – ICT services provider
Eaton`s 9395 UPSs are helping the award winning Walhalla data centre achieve 99.995 per cent availability
En savoir plus ...
7/18/2013
STX Finland – MS Viking Grace cruise ferry
The total capacity of the UPS systems aboard the new vessel was more than 200 kVA. All of the UPSs chosen for this project are versions which have been optimised for marine applications and which have already gained a strong reputation for performance and reliability aboard sea-going vessels in every part of the world.
En savoir plus ...
6/11/2013
Markley – Colocation provider
Power Xpert 9395 units deliver high reliability, efficiency at mission-critical data center facility.
En savoir plus ...
5/1/2013
Williams – Energy infrastructure provider
Power Xpert 9395 delivers high reliability, efficiency for natural gas transporter.
En savoir plus ...
5/1/2013
Sentrum – Colocation provider
Sentrum needed a UPS installation that would combine exceptional reliability with versatility and the highest possible level of energy efficiency.
En savoir plus ...
9/17/2012
Iliad Group – Data centre operator
During the modernisation of its 5,000 m2 DC2 site in Vitry, Paris, Iliad Datacenter needed a reliable UPS installation that would enable the company to increase its energy efficiency without compromising on service quality.
En savoir plus ...
8/17/2012
Royal Institute of Technology – Technical University
Uninterrupted research and unprecedented energy saving at KTH
En savoir plus ...
6/6/2012
Previder – ICT services provider
Dutch ICT service provider Previder offers spacious, ultra-modern and energy-efficient data centres that meet the needs of today and tomorrow. At their new data centre in Hengelo, everything concerning power supply and security is done twice or often even three times over. To ensure uninterrupted, 24/7 availability, the company chose Eaton as their electrical supply system provider.
En savoir plus ...
9/28/2011
Stadtwerke Flensburg – Utility services provider
German utility company Stadtwerke Flensburg is constantly developing new areas of activity. In 2010 they set up a modern, energy-efficient data centre large enough to not only host the servers for the company’s own applications, but also to allow data centre space to be leased out.
En savoir plus ...
5/16/2011
Skåne University – Hospital
Eaton´s power quality solutions contribute to maintaining the Skane University hospital´s vital functions in Malmö, Sweden.
En savoir plus ...
3/30/2011
Royal Caribbean – Allure of the Seas cruise ship
Eaton delivered over 20 doubleconversion, online marine UPSs to the ship. On board the ship is the first ever marine application of Eaton’s Energy Saver System (ESS) technology, which enables the UPS devices to reach an industry-leading efficiency level of 99 per cent.
En savoir plus ...
3/21/2011
Global Switch – Colocation provider
Leading data centres need leading power protection.
En savoir plus ...
2/7/2011
Bahnhof – Internet service provider
The centre relies on Eaton’s UPS protection to provide rock-solid network operations and colocation services.
En savoir plus ...
8/5/2010
IBM – Portable modular data center
Eaton has been chosen as one of the power management partners for IBM’s Portable Modular Data Center (PMDC) solution.
En savoir plus ...
8/5/2010
North Estonia Medical Centre – Hospital
The North Estonia Medical Centre chose Eaton UPSs to protect its patients’ lives.
En savoir plus ...
8/5/2010
Donbass Arena – Football stadium
Donbass Arena has several server and communication rooms that manage the stadium’s IT infrastructure. A total of 35 midand high-range Eaton UPSs provide uninterruptible power.
En savoir plus ...
1/20/2010
Royal Caribbean – Oasis of the Seas cruise ship
Eaton supplied more than 20 double-conversion online UPSs for this giant of the seas.
En savoir plus ...
1/20/2010
Citi – Financial services provider
Global financial services company Citi chose Eaton 9390 UPSs to protect its Barcelona Sales and Services Centre from potentially damaging power losses.
En savoir plus ...
1/14/2010

Latest successes

Landsvirkjun works with Eaton to bring reliable and environmental reserve
Landsvirkjun, the National Power Company of Iceland, is Iceland’s largest electricity generator and one of the ten largest producers of renewable energy in Europe. Landsvirkjun operates 18 power plants in Iceland, and they also operate two windmills as a research and development test site.

Eaton UPS in CE Colo data center environment
In 2015, CE Colo started to address the technological renovation of the existing UPS system. Two independent manufacturers capable of delivering technologies that are required for the challenging data center environment were selected. The reconstruction of the existing functional system required the implementation of a new solution to prevent the renovation from having any impact on the 24/7 operation and the customers.

Informations liées
Revue de presse