Sioux Falls, S.D., USA
Colocation/Web Hosting Services
When this colocation firm began planning an expansion into unused space within its facility, the search was on for a high-availability UPS that could keep pace with rapid growth.
Eaton 9395
A thorough review of available technologies from leading UPS vendors showed the Eaton 9395 as the clear winner, offering unprecendented power perfromance, reliability and efficiency.


CoSentry tripled its client base in the previous two years and needed a UPS that could keep pace with the firm's rapid growth, deliver the highest level of availability and contribute to its energy efficiency effort. In addition to reliability, price point was at the forefront of the organization's prerequisite list.

With CoSentry's 500 kVA 9395 unit configured with two 250 kVA UPMs, the firm benefits from redundancy, modularity, reliability and industry-leading efficiency.

Download the full story

See more success stories