Iliad Group – Data centre operator

Paris, France
Data Centre
During the modernisation of its 5,000 m2 DC2 site in Vitry, Paris, Iliad Datacenter needed a reliable UPS installation that would enable the company to increase its energy efficiency without compromising on service quality.
Five Eaton 9395 550 kVA UPSs, with a total capacity
of 2,500 kW, featuring Energy Saver System (ESS) mode and Variable Module Management System (VMMS) technology, as well as Eaton’s Powerware
Hot Sync® technology.
Energy efficiency increased to 98% from 92%.

Iliad Datacenter is a subsidiary of the Iliad Group and one of France’s largest data centre operators. The company designs and builds all of its own data centres and is a highly regarded operator that prides itself on the quality and security of its services It has a number of major sites in the Paris region, including a 5,000 m2 site in Vitry, and is also currently investing in a major new 11,800 m2 site.
Download the full story

See more success stories