Sentrum – Colocation provider

Location:
United Kingdom
Segment:
Data Centre
Problem:
Sentrum needed a UPS installation that would
combine exceptional reliability with versatility and
the highest possible level of energy efficiency.
Turnkey Solution:
A system based on Power Xpert 9395 UPSs
configured to provide N+N A/B redundancy. Eaton was
also responsible for delivery to the site, installation and commissioning. In adition Eaton provides 24/7 support
for the installed equipment.
Results:
The Eaton UPS system met all of Sentrum’s requirements, with the company being particularly impressed by the modularity and scalability of the Eaton equipment, the high power rating it offers in a small footprint, and the exceptional levels of efficiency and reliability it delivers.

Share
Leading data centre owner and operator Sentrum has several data centres across the UK totalling over 130 000 m2 of space including technical space, disaster recovery suites and offices.
Sentrum was the first operator to offer fully bespoke and scalable solutions with a dedicated plant for every data suite. The company offers customised solutions that meet the highest specifications and enable clients to tailor every aspect of their data suite – including the power and technical configurations – to suit their individual business requirements.
Download the full story

See more success stories