Super Computer

The Finnish IT Centre for Science protects one of the most powerful super-computers in Europe with Eaton’s Powerware UPS

The Finnish IT center for science, CSC, selected Eaton’s UPS solutions for its new supercomputer’s data centre. The supercomputer’s power supply and data centre cooling are secured with Powerware 9395 UPS devices, the most powerful and efficient device of its kind on the market.

Finnish scientists have been presented with a supercomputer that will take the available computing power to a completely new level in the spring of 2008. This enhanced computing power enables the scientists to study phenomena that were previously out of their reach. The Finnish supercomputer has been ranked as one of the most powerful supercomputers in Europe. In the final configuration, the theoretical top performance surpasses 70 Tflops.

The system has a power consumption mode that places particular demands on the power supply and data centre cooling. The computer takes 20 racks of space, and uses 420 kilowatts of power. The essential requirements for the UPS were technical quality, good efficiency rate and dependable maintenance.

Eaton delivered a three 550 kVA Powerware 9395 UPS units to protect the supercomputer. The uninterrupted power supply to the cooling system is secured with two 275 kVA Powerware 9395 units.

”Powerware 9395 is a true tour de force of Eaton’s R&D engineers. It is the first UPS system in its power class that incorporates two UPS units in one device. The system benefits from the Eaton developed and patented parallel Hot Sync® wireless paralleling technology, which enables dividing the system into two completely redundant parts. The Powerware 9395 is Eaton’s most powerful UPS, and no one has offered as reliable a power supply so far,” tells Jari Nieminen, Eaton’s product manager.

CSC in brief

CSC, the Finnish IT center for science, is a non-profit company that provides IT support and resources for academia, research institutes and companies: modeling, computing and information services. CSC offers Finland's widest selection of scientific software and databases and the most powerful supercomputing environment in the country that researchers can use via the Funet network.

ARTICLES
E-mail this page Print this page
Copyright ©2009 Eaton Corporation.
All rights reserved.