Foreseer Advanced Applications
Load Balancing
A major contributor to harmonic
distortion is improper load balancing. Foreseer Class is able to track
load levels by phase, so a user can see or be instantly notified
when extreme imbalances begin to occur, giving users the
knowledge to take the steps necessary to re-distribute the load
before a catastrophic problem can occur. Foreseer Class visually
illustrates the load balance on a device or system in a real
time while showing what the balanced model should be. You see
the current state, the worst case scenario and the proper load.
Electrical Capacity Planning
Planning electrical usage and
demand is difficult at best. As site loads increase and usage
patterns change, demand on a particular device may grow beyond its
intended capacity. And while average demand may not be a concern,
peak demand is of the utmost importance. Even a momentary spike over
the rated capacity could bring down an entire network. Foreseer Class not
only tracks the kW and kVA over time, but immediately informs the
user of peak levels and can project future demands based on past
usage, for periods as long as years or as immediate as minutes. This
knowledge is invaluable in planning for electrical upgrades and/or
changes to the power train to support changing load patterns. Simply
put, Foreseer Class makes understanding power capacity and power density
an easy process.
Power Density
As racks proliferate and expand from TCP/IP networks, with
servers and other elements of the infrastructure placed into smaller
areas, power density has become a critical measurement. Foreseer Class
manages power density by device, for a single rack or the entire
area.
Energy Allocation
The spiraling cost of energy has always been of significant
concern to CFOs, CIOs and CEOs. With information technology as
the lifeblood of companies in the 21st century, balancing cost to
return is a non-trivial task. Foreseer Class provides balance to the
analysis by providing knowledge-based decisions on energy usage for
your information technology. Foreseer Class can provide you with energy
usage by individual circuit so each device can be a part of the
energy management strategy, and can even allocate electrical cost to
the individual users of a department, device or even an individual
or branch circuit.