Power & Product Glossary
ABM
A three-stage charging system designed to prolong the service life
of UPS batteries. By charging the batteries only when necessary,
battery life is significantly improved. Charging stage one:
quickly recharges battery to approximately 90% of capacity.
Charging stage two: fully charges the battery to 100%. Charging
stage three: rest mode prevents overcharging. Charging stage one
is initiated after a power outage or periodic UPS self-test.
AC
Alternating Current electrical power supplied by a utility company
or from an AC generator.
AC Distributon
A module in the Powerware power system that distributes AC power to
other Powerware power system modules.
AC Metering
Measurement of AC power input voltage and current parameters by
sampling. The results of the measurements are used to calculate
the rms equivalents for voltage, current and power, and also
calculate the power factor and frequency.
AC Utility
The electric power furnished by an electric power utility company.
Active Load Share
A current sharing scheme controlled by the supervisory module that adjusts the output voltage of individual rectifiers so that all rectifiers in a DC power system produce the same output current.
Active Voltage Control
The supervisory module adjusts the rectifier output voltages to maintain a constant DC power system voltage (measured at the output or battery) independent of load fluctuations during normal operation.
Agent
A software program that acts as a focal point for data collection
and configuration of a specific network entity (hardware or
software). SNMP agents provide data to management stations
regarding the operation and configuration of devices on a network.
Alternating Current (AC)
Current which changes (or alternates) direction at regular
intervals. Since the current flows in one direction for the same
amount of time that it flows in the opposite direction, the
average value of the current flow is zero.
Ampere (Amp or A)
The unit of measure for current. One ampere is the amount of
electricity per second that flows through a conductor such as a
wire.
AVC
Active Voltage Control
Bandwidth
The data a cable can carry measured in bits per second (bps).
Battery Backup
A battery or a set of batteries in a UPS system. Its purpose is to
provide an alternate source of power if the main source is
interrupted.
Battery Capacity
The battery ampere-hour capacity at full charge, standard
temperature, and at a specified (usually C10) discharge rate.
Battery Charger
A device or a system which provides the electrical power needed to
keep the battery backup fully charged.
Battery Current Limit
System voltage control that limits the battery charge current to a
preset value.
Bi-Directional Converter
A device which changes (or converts) alternating-current power to
direct-current power and vice versa.
Blackout
A total loss of the AC utility (commercial power).
Boost
See buck and boost.
Brownout
A reduction in the voltage of the AC utility without complete loss
of power.
Buck and Boost
A proprietary voltage regulation process used when an overvoltage
or undervoltage situation occurs in the UPS. Undervoltage is
boosted to make the voltage greater, and overvoltage is bucked to
reduce it. The result is less reliance on the UPS battery,
extending overall battery life.
Bus Voltage
The actual voltage supplied to the load as measured at the bus
bars.
Bypass
A circuit used to change the path of the electrical power so that
it goes around (or bypasses) its normal path. In the UPS, the
bypass circuit is used to route the power around the major
electronics in the UPS so they can be serviced without power
interruption.
C10
Symbol for ampere-hour capacity of a battery at the 10-hour
discharge rate, to a specified end voltage.
CE
Conformite Europeene (European Conformity)
Circuit Breaker (CB)
A device for manually opening (breaking) or closing a circuit to
interrupt or apply electric power to an electrical apparatus. A
circuit breaker can also open a circuit automatically when it
senses an overload.
Clean Power
Electrical power which has been conditioned and/or regulated to
remove electrical noise from the output power.
Configuration file
The information or data loaded into and the supervisory module
that controls the behavior of an Powerware power system to suit the
particular requirements of a customer's site or installation.
Configurations Database
This is the total set of configurable parameters.
Conformite Europeene (European Conformity)
CE marking is used to signify that a product complies with all the
applicable performance and safety standards adopted by the members
of the European Union and is therefore certified for sale in
European Union countries.
Converter
A device which changes electrical energy from one form to another,
such as from alternating current to direct current.
Current
Amount of electricity that flows through a conductor, such as a
wire.
Current Share
A process used to balance output currents between rectifiers. See
Active Current Share.
DC
Direct Current
DC Distribution (DCD)
A module in the Powerware power solution that distributes DC power to
the loads. It also provides protection for the load cables.
DC Distribution - Fused version (DCF)
A DC Distribution module that uses fuses for protection.
DC Distribution - Miniature Circuit Breaker (MCB) version (DCM)
A DC Distribution module that uses miniature circuit breakers for
protection.
Delta Connection
A method of connecting a three-phase source or load in series for
a closed circuit (3-wire, plus ground).
Digital Input
An input which recognizes an open-circuit and short-circuit.
Digital Output
A voltage free relay contact.
Direct Current (DC)
A type of current which never reverses its direction. Since the
current flows in only one direct on, the average value of the
current cannot be zero unless the current has stopped flowing.
Double-Conversion
A UPS design in which the primary power path consists of a
rectifier and inverter. Double-conversion isolates the output
power from all input anomalies such as low voltage, surges and
frequency variations by converting AC to DC to AC. See Online UPS.
Dry Contact
Isolated contacts through which the end user supplies an external
circuit. Dry contact UPSs provide basic communication capabilities
such as monitoring and shutdown.
Efficiency
The ratio of the output power from the UPS to the input power from
the utility. This shows the percentage of the input power that is
available as useful output power. For example, a UPS that is 95%
efficient delivers 95% of the utility power it receives to the
load. The remaining power takes the form of dissipated heat.
EMC
Electro Magnetic Compatibility.
Emergency Shutdown
Used to instantly or quickly shutdown all of the electrical power
available to the UPS and the load. An emergency shutdown device is
usually used during a crisis to prevent damage to the UPS and the
load. Some computer-room installations require a Remote Emergency
Power Off (REPO) capability as part of their security/safety
system.
Equalize
This is the process of increasing the Float Voltage to the
Equalize Voltage to recharge or equalize the batteries.
Event
An alarm activation or de-activation.
Fast Charge
Increasing the Operating Voltage after a battery discharge,
following an AC failure, to give a rapid battery recharge.
Fault Tolerance
The ability of a system to continue operating in the event of a
fault.
Filtering
A method of removing noise from the output of a UPS preventing "dirty
power" from reaching connected equipment.
Float Voltage
The set output voltage of the DC power system (not including
temperature compensation or other adjustments).
Frequency
The number of cycles (oscillation positive and negative) completed
in one second. Defined as Hertz (Hz). In North America, utility
power completes 60 cycles per second,(60 Hertz).
Full Load
The greatest load that a circuit is designed to carry under
specific conditions; any additional load is considered an
overload.
Graphic User Interface (GUI)
A computer system using graphics images on the screen rather than
text to display applications information for the user. As used in
the PowerManager software.
Ground (GND)
A conductor connected between a circuit and the soil.
Hardware Default Voltage
The rectifier output fail-safe operating voltage used if the
rectifier microprocessor fails.
Hardwired
Describes any equipment connected to its power source by hardware
attached directly to terminal blocks or distribution panels.
Harmonic Distortion
The presence of harmonics that change the AC voltage waveform from
a simple sinusoidal to complex waveform. Harmonic distortion can
be generated by a load and fed back to the AC utility line,
causing power problems to other equipment on the same circuit.
Heterogeneous Network
A network with a multitude of workstations, and operating systems,
and a variety of application types from different vendors.
High Rupturing Capacity (HRC) (fuse)
A precisely rated fuse which will operate under high fault current
conditions, without self-destructing.
Homogeneous Network
A network of components - workstation, server, operating system
from the same vendor, or compatible equipment that can run under
the same network or operating system.
Hot-Swappable Batteries
A feature which enables the user to change UPS batteries without
powering down the connected load.
Hot-Swappable Power Modules
A feature which enables the user to change UPS power modules
without powering down the connected load.
I/O
Input/Output
Input Line Cord
The covered bundle of wiring connected to the input terminals of
the UPS. The end of the cord not connected to the UPS is
connected, via an input plug, to an AC utility outlet supplying
power to the UPS.
Input Plug
Connected to the end of the input line cord. To be plugged into an
AC utility outlet receptacle.
Internal Bypass
UPS circuitry which provides a redundant power path. If there is
an internal UPS fault, the connected load will still be supplied
with unconditioned utility power.
Inverter
A machine, device, or system that changes direct- current power
into alternating-current power.
Isolation
The separation (often through the use of an isolation transformer)
of one section of a system from undesired electrical influences of
other sections.
Isolation Transformer
A multiple-winding transformer with physically separate primary
and secondary windings. Although the two windings are physically
disconnected, the magnetic field in the windings of the primary
creates (induces) electrical power in the secondary winding. In
this way the electrical power available at the input can be
transferred to the output. An isolation transformer does not
transfer unwanted noise and transients from the input circuit to
the output windings. This attenuation, or reduction in amplitude,
could be as high as one million to one.
LCD
Liquid Crystal Display
LEDs
Light Emitting Diodes located on the front of the UPS that inform
users of various power conditions and UPS operations.
Line-interactive
A UPS containing an off-line inverter that must transfer on during
a blackout, but provides faster transfer times than an off-line
UPS. Power conditioning and surge suppression are provided to
protect the connected load.
Load
Equipment that receives power from a UPS.
Load Bus
The bus to which the Load equipment is connected.
Load Segments
Groups of receptacles on the rear panel of a UPS which can be
independently controlled.
Load Shedding
The ability to selectively shut off a set of UPS output
receptacles, extending the capacity of the UPS battery. Some
Powerware UPS models are able to shed less critical loads by
turning off selected output receptacles during an extended power
failure while maintaining power to the more critical load(s) on
the remaining output receptacles.
Low Voltage Disconnect (LVD)
A module in the Powerware power system that disconnects the load
from the batteries from the when the battery voltage falls below a
preset value. The LVD reconnects the load to the batteries when
the battery voltage rises above a preset value.
Management Information Base (MIB)
The structure of the database in an Powerware power system.
Manual Bypass Switch (MBS)
A manually operated transfer switch used to bypass the major
electronics in the UPS, so the UPS can be serviced without power
interruption.
Mapping
The process of assigning physical entities to logical entities,
e.g. when a particular analogue channel (internal or external) is
assigned to be the channel used for measuring the bus voltage.
Maximum System Current
The maximum current that can be supplied by from an Powerware Power
System (excluding batteries) under all conditions. Normally 120%
of Rated System Current.
MCB
Miniature Circuit Breaker. A precisely rated, resettable circuit
protection device.
MOV
Metal Oxide Varistor. A non-linear semiconductor device used for
surge protection or voltage limiting.
National Electrical Code (NEC)
The code of standards and practices for the U.S. electrical and
electronics industry. Developed by the National Fire Protection
Association of Quincy, Mass. First published in 1896.
Network Transient Protector
An in and out RJ11 jack for telephone/modem protection (120V
models only) or RJ45 for 10Base-T network cable. It isolates
connected equipment such as modem and fax machines from “back
door ”power surges.
Noise
Random, sporadic, or multi-frequency electrical signals that
become part of a transmission making the signal or information
more difficult to identify.
Nominal System Voltage
The DC output voltage generally used to describe a type of system,
usually 24 V or 48 V.
Nominal Value
A designated value which has been accepted for the sake of
convenience. For instance, nominal voltages are values assigned to
circuits so that the voltages of the circuits can be conveniently
discussed as 120 Vac nominal units, or 230 Vac nominal units.
Null Modem Cable
A special cable for connecting two RS-232 ports or devices
directly, in place of a modem connection.
N+X UPS Redundancy
This form of redundancy provides reliable UPS operation by
eliminating any single point of failure within the UPS.
Off-line UPS
A UPS type which feeds power to the load directly from the utility
and then transfers to battery power via an inverter after utility
drops below a specified voltage. The delay between utility power
loss and inverter startup can be long enough to disrupt the
operation of some sensitive loads. Also called a standby UPS.
Online UPS
A UPS in which the inverter is on during normal operating
conditions supplying conditioned power to the load through an
inverter or converter that constantly controls the AC output of
the UPS regardless of the utility line input. In the event of a
utility power failure, there is no delay or transfer time to
backup power.
Outlet
Any point on a wiring system where current is taken to supply
electrical power for a load.
Output Enable Delay
The delay between the start of primary side switching and the
start of output current walk in. This is in two parts: a fixed
hardware delay controlled by the secondary side control circuits
and an adjustable delay controlled by the microprocessor. During
this period the output voltage is at the minimum of approximately
40 V.
Overload
A condition in which the load wants more from the power source
(such as a UPS) than the power source has been designed to supply.
Overvoltage Shutdown (OVSD)
A protection method that will shutdown any rectifier module with
an output voltage over a preset maximum value.
Parallel Online UPS
Online UPS technology that provides redundant sources of
conditioned backup power so that the critical load is protected
even in the event of UPS component failure.
Power Factor (PF)
The ratio of total real power, (W) to the total apparent power in
volt-amperes (VA);W/VA.
Power Management Software
Provides monitoring and shutdown for UPS and connected load.
Power System
A rack module, single rack or several parallel connected racks,
providing DC power to a single DC bus.
Preset Voltage
The voltage that a rectifier will default to if communications
with the Supervisory Module is lost. Generally, this is set to the
float voltage by the Supervisory Module.
PSTN
Public Switched Telephone Network
Rackmount UPS
UPS that can be mounted in a rack along with servers, hubs, and
other devices.
Rated Rectifier Current
The maximum output current of a rectifier at 58V for a 48 V
(nominal) rectifier, or 29 V for a 24 V (nominal) rectifier.
Rated System Current
The sum of the rated rectifier currents in the Powerware power
system.
Raw Power
Electrical power which may or may not contain unwanted electrical
signals.
Receptacle
A contact device installed at an outlet designed to accept a
single plug. Receptacles on the rear of a UPS accept plugs from
supported system equipment such as computers or monitors.
Rectifier
A module fitted to the Powerware power system that converts AC input
power to regulated DC output power.
Rectifier Bus
The bus to which the outputs of the rectifiers are connected.
Rectifier Magazine
A module in the Powerware power system used to connect the
rectifiers to other modules in the Powerware power system.
Rectifier Voltage
The voltage to which the rectifiers are set. This is assumed to be
the same for each rectifier and does not include current share
adjustments.
Redundancy
Duplication of elements in a system or installation to enhance the
reliability or continuity of operation.
Regulation
A method of limiting voltage to a narrow range.
Reserve
Battery time remaining to end of discharge
RFI
Radio Frequency Interference
RM
Rectifier Magazine
RS-232
Also called serial ports; a method of communicating digital
information in which the data bits are transmitted sequentially
over one line.
RS-232C
A common point-to-point hardware configuration for serial
communications.
RS-485
A multidrop hardware configuration for serial communications.
There is no intrinsic method of bus collision detection in RS-485,
so higher layers in the protocol stack must take this into
account.
Scalable UPS
A UPS that allows for expandability; for example, enables a UPS to
accommodate a larger load by purchasing additional power modules.
Simple Network Management Protocol (SNMP)
A request-response protocol that collects management information
from network devices and provides a way to set and monitor
configuration parameters.
Sine Wave
The sinusoidal wave form exhibited by alternating current.
Single-Phase Power (1Ø)
Power that is provided by a single source which normally includes
one hot lead and a grounded return line (neutral).
Slope Discrimination Method
A scheme that causes the Overvoltage Shutdown set point to fall
with increasing load.
SNMP
Simple Network Management Protocol
Square Wave
Output waveform generated by very basic, low-cost UPSs. Functions
adequately for less sensitive loads, but may not provide
acceptable quality input for some types of electronic equipment.
Standby Power System
See Off-Line UPS.
Start-On-Battery
Enables user to power up UPS in the absence of utility power.
Start Up Delay
The interval between power on and the start of current walk in. It
is the sum of the Primary Enable Delay and the fixed and
adjustable portions of the Output Enable Delay.
Status LEDs
Light Emitting Diodes (LEDs) that show the status of the UPS when
they light up or turn off.
Step Wave
(Modified Sine wave) Enhanced version of square wave that provides
adequate input for some more sensitive loads, but still not as
high quality as a sine wave.
Supervisory Module
The module that monitors and controls the operation of the DC
power system.
Surge
A transient (or momentary) wave of current, potential, or power in
an electric circuit.
System Voltage
The nominal voltage of the Powerware power system, equal to the
nominal voltage of the rectifier modules. 48 V or 24 V.
Temperature Compensation
Adjustment of the rectifier output voltage to provide the optimum
charging voltage for the battery. One of the components in system
voltage control, calculated by the Supervisory Module calculation
based on battery temperature.
Temperature Sensor
A sensor that is used to produce a variable electrical output
representing the temperature of a component, typically a battery.
Terminal Block
An insulating base equipped with terminals for connecting
secondary and control wiring. Used on hardwired equipment, such as
a UPS, when input plugs and output receptacles are either
impractical or unavailable.
Terminal
A connector for attaching a conductor to an electrical apparatus.
Three-Phase Power (3Ø)
Power that is provided by a single source with three outputs with
a phase difference of 120 ° between any two of the three voltages
and currents.
Transfer Switch
A switch which will transfer current from one circuit path to
another without interrupting the flow of the current.
Transformer (T)
A device that raises or lowers the voltage of an alternating
current electrical source.
Transient
The fast radical change in a smooth sine wave that occurs in both
voltage and current waveforms during the transition from one
steady-state operating condition to another.
Trickle Charge
With the trickle charging process, the battery receives a constant
voltage feeding a low current. Constant use of this method dries
the electrolyte and corrodes the plate, reducing potential battery
service life by up to 50 percent.
Two-Phase Power
Power which is provided by a single source with two outputs which
may be 180 degrees out of phase or 120 degrees out of phase.
UL
Underwriters Laboratories. An approval organisation based in the
United States.
Uninterruptible Power System (UPS)
A system designed to automatically provide power, without delay or
transients, when the normal power supply is incapable of supplying
acceptable power. Some UPSs also filter and/or regulate utility
power.
UPS Topology
Overall term describing the internal circuitry of a UPS. There are
three basic UPS topologies: standby (off-line), line-interactive,
and online.
User-Replaceable Batteries
User replaceable batteries allow the user to easily exchange UPS
batteries, once the unit has been turned off.
Volt (V)
The unit of measure for voltage. Voltage is the electrical
pressure which forces the current to flow in a conductor such as a
wire.
Volt-Ampere (VA)
Voltage (V) multiplied by the current (ampere); apparent power.
For instance, a device rated at 10 amps and 120 V has a VA rating
of 1200 or 1.2 kVA.
Walk-In-Time
The time that the rectifier takes to reach rated output current
after the Start Up Delay. The slope is fixed so that a lower
output current will have a shorter walk in period.
Walk-In
The process of gradually ramping up rectifier output voltage (and
current) at start up to prevent a large input current surge.
Watt (W)
The unit of measure for true power. Watts = VA x Power Factor
Wye Connection
A three-phase source of load connection, with a single common
junction and three phase lines out or in.
Product List

- PC, Workstation & Home AV UPS
- Eaton 3S (550-700 VA)
- Eaton Ellipse ECO (650-1600VA)
- Eaton 5E (500-2000VA)
- Eaton 5V (650-1050 VA)
- Eaton 5S (550 - 1500VA)
- Eaton 5L (650-1200VA)
- Eaton Ellipse PRO (650-1600VA)
- Network & Server
- Eaton 5SC (500 - 1500VA)
- Eaton 5P (650-1550 VA)
- Eaton 5PX (1500-3000 VA)
- E Series DX (1-3 kVA)
- Eaton DX-RT (6 -10 kW)
- Eaton 9E (1000-3000 VA)
- Eaton 9SX (700VA-11 kVA)
- Eaton 9PX (1-3 kVA)
- Eaton 9PX (5-11 kVA)
- Eaton 9E (6-20 kVA)
- Eaton 9155 (8-30 KVA)
- Eaton 9SX (15kVA-20kVA)
- Data Center & Facility UPS
- Eaton 93E XL (10-40 kVA)
- BladeUPS (12-60 kW)
- Eaton 91PS and 93PS (8-30/40 kW)
- Eaton 93PR (25-200 kW)
- Eaton 93E (100-200kVA) HE UPS
- Eaton 93E (15-500 kVA)
- Eaton 93PR (500-600 kW)
- Power Xpert 9395P (250-1200 kVA)
- Power Xpert 9395 (225-1100 kVA)
- Eaton Micro Data Center
- Marine & Offshore UPS
- Eaton 9130 Marine (1000-3000 VA)
- Eaton 9PX Marine (1500-3000 VA)
- Eaton EX Marine (1500-3000 VA)
- Eaton 9155 Marine (8-30 kVA)
- Eaton 9355 Marine (8-40 kVA)
- Power Xpert 9395 Marine (225-1100 kVA)
- DC Power