Eaton Customer Success Stories from around the World

Customers around the world depend on UPS, services and power quality solutions from Eaton to keep their applications up and running without interruption. Read more about how customers rely on Eaton every day in our latest success stories.

Filter by...

All Success Stories

Title Date
Eaton UPS in CE Colo data center environment
In 2015, CE Colo started to address the technological renovation of the existing UPS system. Two independent manufacturers capable of delivering technologies that are required for the challenging data center environment were selected. The reconstruction of the existing functional system required the implementation of a new solution to prevent the renovation from having any impact on the 24/7 operation and the customers.
Learn more...
4/15/2019
Landsvirkjun works with Eaton to bring reliable and environmental reserve
Landsvirkjun, the National Power Company of Iceland, is Iceland’s largest electricity generator and one of the ten largest producers of renewable energy in Europe. Landsvirkjun operates 18 power plants in Iceland, and they also operate two windmills as a research and development test site.
Learn more...
4/8/2019
New UPS and supercapacitor technology at the heart of hospital
The Pirkanmaa Hospital District (PSHP) worked with Eaton to install modern UPSs with supercapacitor technology to ensure uninterruptible operation of hospital imaging devices.
Learn more...
2/25/2019
Eaton and Amdocs collaborate to create an efficient data center
“The outstanding efforts of Eaton and Carter Sullivan made it possible to complete the Amdocs data center on schedule and on budget”
Learn more...
2/4/2018
CityServiceValcon with Nutanix Hyperconverged
Eaton`s hyperconverged infrastructure solution allows CityServiceValcon to have continuous uptime in their virtualized environment
Learn more...
8/23/2017
Eaton provides Webaxys’ new eco-designed data center with a complete energy storage and management system

Webaxys is a hosting company and telecom operator located in Normandy, France. Since its inception in 2003, the company has pursued a strategy of innovation based on strong values of social engagement and respect for the environment.


Learn more...
11/20/2016
Eaton enables always-on operations for 100 percent renewable power data center
Verne Global owns and operates a 44-acre data center campus in Keflavik, Iceland. The strategic location provides availability to the world’s two largest data center markets, Europe and North America, while also addressing some of the most critical challenges facing today’s data center landscape.
Learn more...
10/13/2016
Eaton garantiert unterbrechungsfreien Service für Total Cloud
Total Cloud vertraut auf die Energiemanagementlösungen von Eaton, die für das Rechenzentrum des Unternehmens von Anfang an einen unterbrechungsfreien Betrieb ermöglichen.
Learn more...
7/18/2016
Lösungen für Rechenzentren von Eaton führen zu Kosteneinsparungen für das Eastbourne College

Mit seinem umfassenden Angebot für das Rechenzentrum stellte Eaton dem Eastbourne College eine integrierte, hocheffiziente Infrastruktur für ein neues Rechenzentrum bereit – und das zur Hälfte günstiger als schlüsselfertige Lösungen anderer Anbieter.


Learn more...
7/18/2016
SAMSØ ferry power system maintains ecological requirements of one of the wonders of the world
Flexible, intelligent and safe power conversion UPS system meets both the environmental and power needs for transport between island and the mainland
Learn more...
4/25/2016
Eaton gives energy efficiency a boost in Meilahti Tower Hospital
Eaton’s reliable UPS devices secure power for the hospital’s mission-critical applications whilst meeting the demand for high energy efficiency, exceeding the set goal of 1-hour+ power continuity.
Learn more...
4/18/2016
Eaton provides BlueFjords data center with power that’s efficient and expandable
The utility power to the BlueFjords data center can be expected to be reliable for the majority of the time thanks to its proximity to the power node. However, power protection is still vital to ensure that the operation of the data center is never disrupted by power problems such as transients, power surges and voltage perturbations.
Learn more...
4/7/2016
Teraco tackles load shedding, efficiency and management issues with Power Xpert 9395 UPS
Teraco was formed to take advantage of large scale deregulation of the telecommunications sector in South Africa, and has grown at an exponential rate, validating their business model; a large proportion of the large enterprises in South Africa rely on Teraco for interconnection services.
Learn more...
9/7/2015
Eaton Prevents Milk Malfunction
The Roshen milk processing plant in Vinnitsa experiences, on average, three to four mains electricity supply failures each quarter. When these failures occur, the effects on the dryers used to convert liquid milk into dehydrated milk powder are costly and disruptive.
Learn more...
6/23/2015
Cinesa – Kinobetreiber

Die Eaton 5PX USV und die Intelligent Power Software  schützen virtualisierte IT-Systeme an 46 Standorten von Cinesa, einer der führenden Kinobetreiber Spaniens.


Learn more...
5/20/2015
E4 Computer Engineering SpA - ICT services provider

Eaton arbeitet mit der italienischen Unternehmung E4 zusammen, um vollkommen eingebaute, messbare und fehlertolerante E4 VSTONE konvergente Infrastrukturlösung für private Clouds zu designen.


Learn more...
5/20/2015
DPC BSTelecom works with Eaton to bring energy efficiency to in demand Russian data
Eaton UPS helped to create a reliable, efficient, trouble-free and cost-effective data center uninterruptible power supply system for BSTelecom.
Learn more...
4/21/2015
Eaton Ensures Reliable and Uninterrupted Operation of Laboratory Equipment for Swiss Pharmaceutical
The Eaton 93PM UPS ensures long-term, reliable and uninterrupted operation of Roche’s laboratory equipment even under heavy load.
Learn more...
4/21/2015
Eaton Powers the Bolshoi Theatre
The Bolshoi Theatre and its warehouse now have a robust power supply system based on Eaton UPS technology.
Learn more...
4/21/2015
Klarer Start-Ziel-Sieg
Die weltweite Nummer 1 in Sachen Isolationsprodukte für elektrische Energie und Verkehrstechnik, die per Stammhaus in Neumarkt am Hausruck ansässige KUVAG Gruppe, ist EDV-mäßig längst auf Virtualisierung eingestellt. Die 9140 USV von Eaton überzeugte hier mit ihrer VMware vSphere 5.1 unterstützenden Intelligent-Power-Software.
Learn more...
5/4/2014
Nachfolge erfolgreich geklärt
Häufige Batteriewechsel, mysteriöse Säureaustritte sowie ein Relais-Versagen waren einem der bedeutendsten europäischen WC-Sitz-Hersteller letztendlich doch zu viel: Eine neue USV-Anlage anderer firmenpolitischer Farbe musste her. Mit der Eaton 9PX war schnell ein würdiger Nachfolger gefunden. Dank Software und VMware Unterstützung ist MKW auch in der virtuellen Welt gerüstet.
Learn more...
5/4/2014
Stimmiges Gesamtpaket
Die Fertigungslinien von Seidel Elektronik, einem beliebten Outsourcingpartner für elektronische und mechatronische Produkte, arbeiten präzise, schnell und nahezu rund um die Uhr.  Zentral geregelte Hochverfügbarkeit dank den redundanten USV 9355-Online-Doppelwandler-Geräte von Eaton.
Learn more...
5/4/2014
Econocom – ICT services provider
Econocom is collaborating with Eaton on the development of viCUBE in relation to racks, intelligent ePDUs, UPSs as well as Eaton´s power management software called Intelligent Power™.
Learn more...
4/1/2014
Virtus – Colocation provider
Virtus Data Centres provides modern and flexible colocation space to support London’s financial, media, cloud and digital businesses. The company’s data centres are designed with both environmental efficiency and high connectivity in mind.
Learn more...
3/9/2014
Facebook – Social networking company
Facebook leveraged the Power Xpert 9395 to help take its Power Usage Effectiveness (PUE) rating to well below the industry average.
Learn more...
2/3/2014
Bakhresa – Milk production plant
Eaton UPS equipment with doubleconversion technology provides the best available protection against all types of power quality problems and offers class-leading efficiencies of up to 99 percent
Learn more...
12/5/2013
ServeisWeb – Internet service provider
The two new UPSs were installed with no downtime and, alongside the existing units, provide continuous, conditioned, reliable electricity enabling ServeisWeb’s level of service to be maintained.
Learn more...
9/24/2013
NURTS Bulgaria – Radio and television broadcaster
NURTS Bulgaria AD identified that it needed to modernise its backup power supplies to ensure its network is thoroughly protected against power outages and operating at the highest level of efficiency possible. With an efficiency rating of over 95 per cent, Eaton 9130 rack mount UPSs were selected for their energy saving potential.
Learn more...
9/3/2013
Granite Networks – Colocation provider
Data center firm achieves 100% uptime with 9395 UPS.
Learn more...
8/17/2013
IDentiphoto – ID technology systems integrator
Firm quick to ID value, efficiency in Eaton 5P.
Learn more...
8/17/2013
Kortek Solutions – ICT services provider
Eaton efficiency, software are stands outs for IT firm.
Learn more...
8/17/2013
Automatia
Eaton gewährleistet eine unterbrechungsfreie Stromversorgung für alle Otto Geldautomaten in Finnland
Learn more...
7/18/2013
Grosses Kino Digiplex
Eaton’s USV-Technologie sorgt dafür, dass die Kinobesucher Ihren Film geniessen können ohne Unterbrechung und das auf kleinstem Raum.
Learn more...
7/18/2013
Tissat
Eaton’s USV 9395 hilft dem preisgekrönten Walhalla Datenzentrum eine Verfügbarkeit von 99.995% zu erreichen
Learn more...
7/18/2013
Sichere Energie für die weltweit umweltfreundlichste Fähre
Gebaut für die finnische Viking Line, ist die revolutionäre MS Viking Grace, die erste Fähre einer neuen Generation, welche von Anfang an entwickelt und gebaut worden ist, um die Umwelt zu schonen.
Learn more...
6/11/2013
Markley – Colocation provider
Power Xpert 9395 units deliver high reliability, efficiency at mission-critical data center facility.
Learn more...
5/1/2013
Williams – Energy infrastructure provider
Power Xpert 9395 delivers high reliability, efficiency for natural gas transporter.
Learn more...
5/1/2013
Sentrum
Führender Rechenzentrum Eigentümer und Betreiber Sentrum benötigte eine USV-Anlage, die außergewöhnliche Zuverlässigkeit, Vielseitigkeit und die höchstmögliche Energieeffizienz für sein Rechenzentrum in Woking UK kombinierte.
Learn more...
9/17/2012
Iliad Datacenter
Während der Modernisierung seines 5.000 m2 DC2 Standortes in Vitry, Paris, benötigt Iliad Datacenter eine zuverlässige USV-Anlage, die es dem Unternehmen ermöglicht, seine Energieeffizienz zu erhöhen ohne Kompromisse bei der Servicequalität einzugehen.
Learn more...
8/17/2012
Royal Institute of Technology (KTH)
KTH, die grösste, älteste und internationalste Universität in Schweden entschied sich für die Eaton USV 9395, um Ihr Computer-Center in Stockholm zu schützen.
Learn more...
6/6/2012
Gambro
Eaton 9395 UPS ensures continuous uptime for medical manufacturer
Learn more...
10/31/2011
Previder konzentriert sich auf Sicherheit
Der holländische ICT-Dienstleister „Previder“ bietet geräumige, hochmoderne und energieeffiziente Rechenzentren, um den Bedürfnissen von Heute und Morgen gerecht zu werden. In ihrem neuen Rechenzentrum in Hengelo, wird alles betreffend Stromversorgung und Sicherheit zweimal oder oft auch dreimal geprüft. Um eine ungestörte, 24/7 Verfügbarkeit zu gewährleisten, entschied sich das Unternehmen, Eaton als Ihren Stromversorgungs-Lieferanten zu nehmen.
Learn more...
9/28/2011
Stadtwerke Flensburg – Utility services provider
German utility company Stadtwerke Flensburg is constantly developing new areas of activity. In 2010 they set up a modern, energy-efficient data centre large enough to not only host the servers for the company’s own applications, but also to allow data centre space to be leased out.
Learn more...
5/16/2011
Skåne University – Hospital
Eaton´s power quality solutions contribute to maintaining the Skane University hospital´s vital functions in Malmö, Sweden.
Learn more...
3/30/2011
Royal Caribbean – Allure of the Seas cruise ship
Eaton delivered over 20 doubleconversion, online marine UPSs to the ship. On board the ship is the first ever marine application of Eaton’s Energy Saver System (ESS) technology, which enables the UPS devices to reach an industry-leading efficiency level of 99 per cent.
Learn more...
3/21/2011
Global Switch – Colocation provider
Leading data centres need leading power protection.
Learn more...
2/7/2011
Bahnhof – Internet service provider
The centre relies on Eaton’s UPS protection to provide rock-solid network operations and colocation services.
Learn more...
8/5/2010
IBM – Portable modular data center
Eaton has been chosen as one of the power management partners for IBM’s Portable Modular Data Center (PMDC) solution.
Learn more...
8/5/2010
North Estonia Medical Centre – Hospital
The North Estonia Medical Centre chose Eaton UPSs to protect its patients’ lives.
Learn more...
8/5/2010
Donbass Arena – Football stadium
Donbass Arena has several server and communication rooms that manage the stadium’s IT infrastructure. A total of 35 midand high-range Eaton UPSs provide uninterruptible power.
Learn more...
1/20/2010
Royal Caribbean – Oasis of the Seas cruise ship
Eaton supplied more than 20 double-conversion online UPSs for this giant of the seas.
Learn more...
1/20/2010
Citi – Financial services provider
Global financial services company Citi chose Eaton 9390 UPSs to protect its Barcelona Sales and Services Centre from potentially damaging power losses.
Learn more...
1/14/2010
Rechenzentrum – vorgesorgt!
Mit dem Neubau ihres Verwaltungsgebäudes realisierten die Stadtwerke Flensburg ein neues und modernes Rechenzentrum. Eaton lieferte dafür ein komplettes Stromversorgungssystem von der Stromverteilung bis zur Netzersatzanlage inklusive Serviceleistungen.
Learn more...
9/14/2009
zenOn und Powerware – Stabile Energieversorgung garantiert
Um für mehr Sicherheit und Zuverlässigkeit zu sorgen, hat sich BMW Regensburg für ein dezentrales Powermanagement entschieden. Neben diesen beiden Aspekten spielten auch Wirtschaftlichkeit und nachhaltiger Nutzen für den Automobilhersteller eine große Rolle. Zusammen mit den beiden Partnern Eaton Powerware und Prozesstechnik Kropf hat BMW Regensburg dieses Projekt umgesetzt.
Learn more...
11/19/2007
Linck HVT
Die Region um Oberkirch im Ortenaukreis wird viele Tage im Jahr von der Sonne verwöhnt – doch gerade in den Sommermonaten gibt es rund um das Städtchen im Schwarzwald auch häufig Gewitter. Das stört die Touristen, die im Sommer in die Weingegend kommen, nicht sonderlich. Doch für das traditionsreiche Unternehmen Linck HVT in Oberkirch hatten diese mit Stromausfällen oder Spannungsschwankungen verbundenen Wetterkapriolen sehr oft negative Folgen.
Learn more...
3/20/2007

Latest successes

Landsvirkjun works with Eaton to bring reliable and environmental reserve
Landsvirkjun, the National Power Company of Iceland, is Iceland’s largest electricity generator and one of the ten largest producers of renewable energy in Europe. Landsvirkjun operates 18 power plants in Iceland, and they also operate two windmills as a research and development test site.

Eaton UPS in CE Colo data center environment
In 2015, CE Colo started to address the technological renovation of the existing UPS system. Two independent manufacturers capable of delivering technologies that are required for the challenging data center environment were selected. The reconstruction of the existing functional system required the implementation of a new solution to prevent the renovation from having any impact on the 24/7 operation and the customers.

Zugehörige Infos
Presse