SAMSØ ferry power system maintains ecological requirements of one of the wonders of the world

Location:
Denmark, Samsø

Challenge:
Deliver an ecologically friendly LNG power system adaptable for ship to shore or shore to ship power use.

Solution:
Power Xpert 9395 Marine UPS frequency converter, EC4P programmable logic controller (PLC).

Results:
Utilization of land-based (50 Hz) power system and ship-based (60 Hz) power system flexibly,  intelligently and safely.

Share
Denmark does not possess fossil fuels and since the 1970s, they have been researching more ecological solutions. In fact Samsø became the symbol of a new energy policy and it is often called “the ecological wonder of the world” as it is the first Danish island to use 100% renewable energy and consequently has a CO2 emissions rating of zero.
Download the full story

See more success stories