Power & Product Glossary
AC
Alternating Current electrical power supplied by a utility company
or from an AC generator.
AC Distribution
A module in the Eaton power system that distributes AC power to
other Eaton power system modules.
AC Metering
Measurement of AC power input voltage and current parameters by
sampling. The results of the measurements are used to calculate
the rms equivalents for voltage, current and power, and also
calculate the power factor and frequency.
AC Utility
The electric power furnished by an electric power utility company.
Active Load Share
A current sharing scheme controlled by the supervisory module that adjusts the output voltage of individual rectifiers so that all rectifiers in a DC power system produce the same output current.
Active Voltage Control
The supervisory module adjusts the rectifier output voltages to maintain a constant DC power system voltage (measured at the output or battery) independent of load fluctuations during normal operation.
Advanced Battery Management
A three-stage charging technique that
automatically tests battery health.
Provides advance notification when
preventive maintenance is needed,
allowing ample time to hot-swap batteries
without ever having to shut down
connected equipment significantly
extending the life of your UPS's battery
(and, quite possibly, your contract).
Agent
A software program that acts as a focal point for data collection
and configuration of a specific network entity (hardware or
software). SNMP agents provide data to management stations
regarding the operation and configuration of devices on a network.
Alternating Current (AC)
An electric current that reverses its
direction at regularly recurring intervals,
as opposed to direct current, which is
constant. Usually in a sine wave pattern,
for optimal transmission of energy.
Ampere (Amp or A)
The unit of measure for the rate of flow
of electricity, analogous to gallons per
minute. VA x 0.7 (power factor) = watts
Apparent Power
Applied voltage multiplied by current in an
AC circuit which doesn’t take the power
factor into account. Unit is volt amperes
(VA).
Arc
Sparking that results when undesirable current flows between two points of differing potential due to leakage through the intermediate insulation or a leakage path due to contamination.
Audible Noise
A measure of the noise emanating from a
device at audible frequencies.
AVC
Active Voltage Control

Backup Time
The amount of time the battery in a UPS
is designed to support the load.
Balanced Load
AC power system using more than two wires, where the current and voltage are of equal value in each energized conductor.
Bandwidth
The data a cable can carry measured in bits per second (bps).
Battery Backup
A battery or a set of batteries in a UPS system. Its purpose is to
provide an alternate source of power if the main source is
interrupted.
Battery Capacity
The battery ampere-hour capacity at full charge, standard
temperature, and at a specified (usually C10) discharge rate.
Battery Charger
A device or a system which provides the electrical power needed to
keep the battery backup fully charged.
Battery Current Limit
System voltage control that limits the battery charge current to a
preset value.
Battery String
A group of batteries connected together
in a series.
Bi-Directional Converter
A device which changes (or converts) alternating-current power to
direct-current power and vice versa.
Blanking Panels
Steel or plastic plates that are inserted in empty U spaces at the front of a rack or enclosure. They are used to improve airflow for the installed equipment and to reduce hot and cold air recirculation and remixing within the rack. Also referred to as filler panels.

Boost
See buck and boost.
British Thermal Unit (BTU)
Used to measure heat dissipation and is
the amount of energy required to raise
one pound of water one degree
Fahrenheit. One pound of water at 32°F
requires the transfer of 144 BTUs to
freeze into solid ice.
Brown Field
An existing data center—often with
limited possibilities for sustainable and
energy-efficient designs.
Brownout
A steady state of low voltage, but not
zero voltage. Brownouts often occur
during summer months when energy use
is high.
Buck and Boost
A proprietary voltage regulation process used when an overvoltage
or undervoltage situation occurs in the UPS. Undervoltage is
boosted to make the voltage greater, and overvoltage is bucked to
reduce it. The result is less reliance on the UPS battery,
extending overall battery life.
Bus Voltage
The actual voltage supplied to the load as measured at the bus
bars.
Busway
Provides flexible “plug and play” power distribution for a variety of applications where change and adaptation are important.

Bypass
A circuit used to change the path of the electrical power so that
it goes around (or bypasses) its normal path. In the UPS, the
bypass circuit is used to route the power around the major
electronics in the UPS so they can be serviced without power
interruption.

C10
Symbol for ampere-hour capacity of a battery at the 10-hour
discharge rate, to a specified end voltage.
Cable Managers
An easily installed device used to manage and protect cables either horizontally or vertically. Vertical managers are available as single- or double-sided, and for the full height of the rack.

Cages
Modular wall systems that can be used to partition white space environments, particularly in a colocation or multi-tenant data center (MTDC).

Canadian Standards Association (CSA)
An independent Canadian organization that tests for public safety, similar to the function of Underwriters Laboratories (UL) in the U.S.
Capacitor
An electronic component that can store
an electrical charge on conductive plates.
CE
Conformite Europeene (European Conformity)
Circuit Breaker (CB)
A device for manually opening (breaking) or closing a circuit to
interrupt or apply electric power to an electrical apparatus. A
circuit breaker can also open a circuit automatically when it
senses an overload.
Charger
An electronic component in a UPS that provides regulated DC voltage to recharge batteries.
Chimney
A structure, usually vertical, containing a passage or flue by which hot air is extracted out of an enclosure.
Clean Power
Electrical power which has been conditioned and/or regulated to
remove electrical noise from the output power.
Cloud Computing
Internet- (cloud-) based development and use of computer technology. This new supplement, consumption and delivery model for IT services typically involves the provision of dynamically scalable, and often virtualized, resources as a service over the Internet.
Common Mode Noise
An undesirable voltage that appears
between the power conductors and
ground.
Commercial Power
The power supplied by local utility
companies which can vary drastically in
quality throughout the U.S. depending on
location, weather and other factors.
Communication Bay
Also known as an option slot, a UPS
feature that enables the addition of various
connectivity cards for Web, SNMP,
Modbus or serial connectivity interface
capabilities.

Eaton 9130 equipped with a communication bay.
Configuration file
The information or data loaded into and the supervisory module
that controls the behavior of a power system to suit the
particular requirements of a customer's site or installation.
Configurations Database
This is the total set of configurable parameters.
Conformite Europeene (European Conformity)
CE marking is used to signify that a product complies with all the
applicable performance and safety standards adopted by the members
of the European Union and is therefore certified for sale in
European Union countries.
Converged Infrastructure
The combination of server, storage, networking, virtualization and sometimes other resources into an integrated solution that is managed as a whole rather than through separate management systems.
Converter
A device that delivers DC power when
energized by a DC source. It’s also a
section of a switching power supply that
performs the actual power conversion and
final rectification.
Crest Factor
Usually refers to current. It’s the
mathematical relationship between RMS
and peak current. A normal resistive load
will have a crest factor of 1.4142, which is
the normal relationship between peak and
RMS current. A typical PC will have a
crest factor of 3.
Critical Equipment
Equipment such as computers,
communications systems or electronic
process controls, which must be
continuously available.
Current
Amount of electricity that flows through a conductor, such as a
wire.
Current Share
A process used to balance output currents between rectifiers. See
Active Current Share.

DC
Direct Current
DC Distribution (DCD)
A module in a DC power system that
distributes DC power to the loads. It also
provides protection for the load cables.
DC Distribution - Fused version (DCF)
A DC Distribution module that uses fuses for protection.
DC Distribution - Miniature Circuit Breaker (MCB) version (DCM)
A DC Distribution module that uses miniature circuit breakers for
protection.
DC Power System
An AC to DC power supply with
integrated control and monitoring, and
standby batteries designed to supply
no-break DC power (usually 24V or 48V)
to telecommunications and IT network
equipment.
Delta Connection
A circuit formed by connecting three
electrical devices in series to form a
closed loop; most often used in three-phase
connections. If you fly Delta
Airlines, this most likely takes place in
Atlanta, Salt Lake City or Cincinnati.
Derating
A reduction of some operating
parameters to compensate for a change
in one or more other parameters. In
power systems, the output power rating
is generally reduced at elevated
temperatures.
Digital Input
An input which recognizes an open-circuit and short-circuit.
Digital Output
A voltage free relay contact.
Direct Current (DC)
An electric current in which the flow of
electrons is in one direction, such as
supplied by a battery.
Double Conversion
A UPS design in which the primary power
path consists of a rectifier and inverter. It
isolates the output power from all input
anomalies such as low voltage surges and
frequency variations.
Downtime –
Use Eaton’s Downtime Calculator to quantify the impact
The time during which a functional unit
can’t be used because of a fault within it
or the environment.
Dry Contacts
Dry contact refers to a contact of a relay
which does not make or break a current.

Efficiency
The ratio of output to input power.
Generally measured at full-load and
nominal line conditions. If the power
efficiency of a device is 90 percent, you
get back 90 watts for every 100 you put
in, and the rest is mainly dissipated as
heat from the filtration process. To think
of it another way, this would be
equivalent to a bartender pouring off
about an ounce and a half of your beer
before handing you the remaining 14.5
ounces!
Electrical Line Noise
Radio frequency interference (RFI),
electromagnetic interference (EMI) and
other voltage or frequency disturbances.
Electromagnetic Interference (EMI)
Electrical interference that can cause
equipment to work improperly, EMI can
be separated into conducted EMI
(interference conducted through cables
out of the UPS) and radiated EMI
(interference conducted through the air).
EMC
Electro Magnetic Compatibility.
Emergency Shutdown
Used to instantly or quickly shutdown all of the electrical power
available to the UPS and the load. An emergency shutdown device is
usually used during a crisis to prevent damage to the UPS and the
load. Some computer-room installations require a Remote Emergency
Power Off (REPO) capability as part of their security/safety
system.
Energy Saver System (ESS) –
Read more here
Innovative technology from Eaton that
enables select UPS models to operate at
99 percent efficiency without
compromising reliability—not to be
confused with inferior “eco” modes.

Eaton Energy Saver System
Environmental rack monitoring (ERM)
This device continuously monitors environmental conditions at the rack level, providing an extra level of security for critical assets. It’s most often found in high-density data centers and applications like healthcare, where the environment must be maintained within acceptable levels.

ePDU –
Read more here
A power distribution unit that mounts to
rack enclosures and distributes power to
connected devices via a wide variety of
output receptacles.
Equalize
This is the process of increasing the Float Voltage to the
Equalize Voltage to recharge or equalize the batteries.
Event
An alarm activation or de-activation.

Fast Charge
Increasing the Operating Voltage after a battery discharge,
following an AC failure, to give a rapid battery recharge.
Fault Tolerance
The ability of a system to continue operating in the event of a
fault.
Federal Communications Commission
(FCC)
A U.S. federal regulating body whose new
EMI limitations are affecting the design
and production of digital electronics
systems and their related subassemblies.
Filtering
A method of removing noise from the output of a UPS preventing "dirty
power" from reaching connected equipment.
Float Voltage
The set output voltage of the DC power system (not including
temperature compensation or other adjustments).
Flooded Batteries
A form of battery where the plates are
completely immersed in a liquid
electrolyte.
Frequency
The number of complete cycles of AC
voltage that occur during one second
(Hz). In North America, electrical current
is supplied mainly at 60 Hz, or 60 cycles
per second.
Full Load
The greatest load that a circuit is designed to carry under
specific conditions; any additional load is considered an
overload.

Graphic User Interface (GUI)
A computer system using graphics images on the screen rather than
text to display applications information for the user. As used in
the Power Manager software.
Green Field
A new data center with many possibilities
for sustainable and energy-efficient
designs.
Ground (GND)
A conducting connection, whether
intentional or accidental, by which an
electric circuit or equipment is connected
to the earth, or to some conducting body
of relatively large extent that serves in its
place.


Hardware Default Voltage
The rectifier output fail-safe operating voltage used if the
rectifier microprocessor fails.
Hardwired
Describes any equipment connected to its power source by hardware
attached directly to terminal blocks or distribution panels.
Harmonics –
View this slideshow to learn more
sinusoidal component of an AC voltage
that’s multiple of the fundamental
waveform frequency. Certain harmonic
patterns may cause equipment problems.
Harmonic Distortion
Regularly appearing distortion of the sine
wave which is converted into a complex
waveform at a multiple of the
fundamental frequency.
Hertz (Hz)
A unit of frequency equal to one cycle per
second.
Heterogeneous Network
A network with a multitude of workstations, and operating systems,
and a variety of application types from different vendors.
High Efficiency Mode
A mode of UPS operation that cuts
energy usage and operating costs..
High Rupturing Capacity (HRC) (fuse)
A precisely rated fuse which will operate under high fault current
conditions, without self-destructing.
High Voltage (HV)
In the context of UPS products, high
voltage is anything ≥200V: 200V, 208V,
220V, 230V, 240V, 250V, 480V and 600V.
High Voltage Spike
Rapid voltage peaks up to 6,000 volts.
Homogeneous Network
A network of components - workstation, server, operating system
from the same vendor, or compatible equipment that can run under
the same network or operating system.
Hot Swappable
The ability to change a module without
taking the critical load off the UPS. Also
see “user replaceable.”

The batteries on this Eaton 9130 UPS are hot swappable.

I/O
Input/Output
Impedance
The total opposition to alternating current
flow in an electrical circuit.
Input Line Cord
The covered bundle of wiring connected to the input terminals of
the UPS. The end of the cord not connected to the UPS is
connected, via an input plug, to an AC utility outlet supplying
power to the UPS.
Input Plug
Connected to the end of the input line cord. To be plugged into an
AC utility outlet receptacle.
Input Voltage Range
The voltage range within which a UPS
operates in “normal” mode and doesn’t
require battery power.
Inrush Current
The maximum, instantaneous input
current drawn by an electrical device
when first turned on. Some electrical
devices draw several times their normal
full-load current when initially energized.
Insulated Gate Bipolar Transistor (IGBT)
A three-terminal power semiconductor
device, noted for high efficiency and fast
switching. It switches electric power in
many modern appliances such as electric
cars, trains and UPSs.
Internal Bypass
UPS circuitry which provides a redundant power path. If there is
an internal UPS fault, the connected load will still be supplied
with unconditioned utility power.
Inverter
UPS assembly that converts internal DC
power to output AC power to run the
user’s equipment. When the inverter is
supporting 100 percent of the load at all
times, as with an online UPS, there is no
break from utility to battery power.
Isolation
The separation (often through the use of an isolation transformer)
of one section of a system from undesired electrical influences of
other sections.
Isolation Transformer
A multiple-winding transformer with physically separate primary
and secondary windings. Although the two windings are physically
disconnected, the magnetic field in the windings of the primary
creates (induces) electrical power in the secondary winding. In
this way the electrical power available at the input can be
transferred to the output. An isolation transformer does not
transfer unwanted noise and transients from the input circuit to
the output windings. This attenuation, or reduction in amplitude,
could be as high as one million to one.

Kilovolt Ampere (kVA)
A common measurement of equipment
capacity equalling 1000 volt-amperes. An
approximation of available power in an AC
system that does not take the power
factor into account.
Kinetic Energy
The energy an object possesses because
of its motion.

LCD
Liquid Crystal Display
LEDs
Light Emitting Diodes located on the front of the UPS that inform
users of various power conditions and UPS operations.
Line Conditioner
A device intended to improve the quality
of the power that’s delivered to electrical
load equipment. A line conditioner is
generally designed to improve power
quality (e.g., proper voltage level, noise
suppression, transient impulse protection,
etc.).
Line Interactive
An offline UPS topology in which the system interacts with the utility line to regulate the power to the load. Provides better protection than a standby system but isn’t as fully prepared against irregularities as a full double-conversion system.
Linear Load
AC electrical loads where the voltage and
current waveforms are sinusoidal. The
current at any time is proportional to
voltage.
Load
The equipment connected to and
protected by a UPS.
Load Bus
The bus to which the Load equipment is connected.
Load Segment
UPS configuration with separate
receptacle groups, enabling scheduled
shutdowns and maximum backup power
time for critical devices.

This Eaton 9130 UPS is equipped with two load segments, each with three 5-15R.
Load Shedding
The ability to selectively shut off a set of UPS output
receptacles, extending the capacity of the UPS battery. Some
UPS models are able to shed less critical loads by
turning off selected output receptacles during an extended power
failure while maintaining power to the more critical load(s) on
the remaining output receptacles.
Low Voltage (LV)
In the context of UPS products, low
voltage is anything <200V (100V and
120V).
Low Voltage Disconnect (LVD)
A module in the power system that disconnects the load
from the batteries from the when the battery voltage falls below a
preset value. The LVD reconnects the load to the batteries when
the battery voltage rises above a preset value.

Maintenance Bypass
An external wiring path to which the load
can be transferred to upgrade or perform
service on the UPS without powering
down the load.
Make-Before-Break
Operational sequence of a switch or relay
where the new connection is made prior
to disconnecting the existing connection,
that’s also know as soft-load-transfer
switching.
Management Information Base (MIB)
The structure of the database in an Eaton power system.
Manual Bypass Switch (MBS)
A manually operated transfer switch used to bypass the major
electronics in the UPS, so the UPS can be serviced without power
interruption.
Mapping
The process of assigning physical entities to logical entities,
e.g. when a particular analogue channel (internal or external) is
assigned to be the channel used for measuring the bus voltage.
Maximum System Current
The maximum current that can be supplied by from a Power
System (excluding batteries) under all conditions. Normally 120%
of Rated System Current.
MCB
Miniature Circuit Breaker. A precisely rated, resettable circuit
protection device.
Modbus
A serial communications protocol that’s
the most commonly available means of
connecting industrial electronic devices. It
allows for communication between many
devices connected to the same network.
MOV
Metal Oxide Varistor. A non-linear semiconductor device used for
surge protection or voltage limiting.

National Electrical Code (NEC)
The code of standards and practices for the U.S. electrical and
electronics industry. Developed by the National Fire Protection
Association of Quincy, Mass. First published in 1896.
Network Transient Protector
UPS feature that isolates networks,
modems and cables from power threats,
including surges and spikes.
Noise
(1) A disturbance that affects a signal; it can distort the information carried by it.
(2) Random variations of one or more characteristics of any entity, such as voltage, current or data.
(3) Loosely, any disturbance tending to interfere with normal operation of a device.
Nominal Output Voltage
The intended, ideal voltage of any given
output.
Nominal System Voltage
The DC output voltage generally used to describe a type of system,
usually 24 V or 48 V.
Nominal Value
A designated value which has been accepted for the sake of
convenience. For instance, nominal voltages are values assigned to
circuits so that the voltages of the circuits can be conveniently
discussed as 120 Vac nominal units, or 230 Vac nominal units.
Non-linear Load
AC electrical loads where the current is
not proportional to the voltage. Non-linear
loads often generate harmonics in the
current waveform that lead to distortion
of the voltage waveform.
Null Modem Cable
A special cable for connecting two RS-232 ports or devices
directly, in place of a modem connection.
N+X UPS Redundancy
This form of redundancy provides reliable UPS operation by
eliminating any single point of failure within the UPS.

Offline
Any UPS that doesn’t fit the definition of online. Line-interactive and standby topologies are offline.
Ohm
The unit of measurement for electrical
resistance or opposition to current flow.
Ohm's Law
The voltage (E) is equal to the current (I)
times the resistance (R). The formula is
written: E=IR.
Online
A UPS that provides power to the load from its inverter 100 percent of the time, regulating BOTH voltage and frequency, usually using double-conversion topology.
Orderly Shutdown
The sequenced shutdown of units
comprising a computer system to prevent
damage to it and subsequent corruption
or loss of data.
Outlet
Any point on a wiring system where current is taken to supply
electrical power for a load.
Output Enable Delay
The delay between the start of primary side switching and the
start of output current walk in. This is in two parts: a fixed
hardware delay controlled by the secondary side control circuits
and an adjustable delay controlled by the microprocessor. During
this period the output voltage is at the minimum of approximately
40 V.
Output Waveform (UPS)
The shape of the graph of alternating
current on the output side of a UPS. The
highest quality of an output waveform
from a UPS is the sine wave, but, some
UPSs provide step waves or modified
sine waves.

Overload
A condition in which the load wants more from the power source
(such as a UPS) than the power source has been designed to supply.
Overvoltage Shutdown (OVSD)
A protection method that will shutdown any rectifier module with
an output voltage over a preset maximum value.

Parallel Online UPS
Online UPS technology that provides redundant sources of
conditioned backup power so that the critical load is protected
even in the event of UPS component failure.
Parallel Operation
The ability of UPSs to be connected
so the current from corresponding
outputs can be combined into a
single load.
Partition
A logical division of a hard disk created
to have different operating systems on
the same hard disk or to create the
appearance of having separate hard
drives for file management, multiple
users, or other purposes.
Peak Demand
The highest 15- or 30-minute demand
recorded during a 12-month period.
Phase
The time relationship between current
and voltage in AC circuits.
Plenum Cable
Cable that’s laid in the plenum spaces of
buildings to facilitate air circulation for
heating and air conditioning systems. The
plenum space is typically used to house
computer and telephone network
communication cables. Cable that runs
between floors in non-plenum areas is
rated as riser cable.
Plug and Play
An electrical device that doesn’t require
extensive setup to operate.

The Eaton 3S UPS has plug and-play capability.
Power Factor (PF)
(1) The ratio of real power to apparent
power. Watts divided by VA. Most power
supplies used in communication and
computer equipment have a power factor
of 0.9.
(PF = 0.9)
VA x PF = W
W/PF = VA
Power Management Software
Provides monitoring and shutdown for UPS and connected load.
Power Sag
Low voltage (below nominal 120 volts).
Power Surge
High voltage (above nominal 120 volts).
Power System
A rack module, single rack or several parallel connected racks,
providing DC power to a single DC bus.
Preset Voltage
The voltage that a rectifier will default to if communications
with the Supervisory Module is lost. Generally, this is set to the
float voltage by the Supervisory Module.
PSTN
Public Switched Telephone Network
Pulse Width Modulation (PWM)
A circuit used in switching regulated
power supplies where the switching
frequency is held constant and the width
of the power pulse is varied, controlling
both lines and load changes with minimal
dissipation.

Rackmount
Ability to mount an electrical assembly into a standardized rack. Generally stacked up to 42U and 19 inches wide.
Rack Unit (U)
A unit of height measurement in a rack
enclosure. A U is equivalent to 1.75
inches.

The Eaton 5PX UPS occupies 2U of rack space and the optional extended battery module also occupies 2U.
Rail Kit
A set of metal brackets that allows the
installation of a UPS or extended battery
module in a 2- or 4-post rack.

Rated Rectifier Current
The maximum output current of a rectifier at 58V for a 48 V
(nominal) rectifier, or 29 V for a 24 V (nominal) rectifier.
Rated System Current
The sum of the rated rectifier currents in the Eaton power
system.
Raw Power
Electrical power which may or may not contain unwanted electrical
signals.
Receptacle
A contact device installed at an outlet designed to accept a
single plug. Receptacles on the rear of a UPS accept plugs from
supported system equipment such as computers or monitors.
Rectifier
A UPS component that converts incoming
AC power to DC power for feeding the
inverter and charging the battery.
Rectifier Bus
The bus to which the outputs of the rectifiers are connected.
Rectifier Magazine (RM)
A module in the DC power system used
to connect the rectifiers in the power
system.
Rectifier Voltage
The voltage to which the rectifiers are set. This is assumed to be
the same for each rectifier and does not include current share
adjustments.
Redundancy
The ability to connect units in parallel so if
one fails the other(s) will provide continual
power to the load. This mode
is used in systems when power failure
can’t be tolerated.
Regulation
A method of limiting voltage to a narrow range.
Relay Communication
Communication between a UPS and
a computer through the opening and
closing of solid-state relays that are
pre-defined to indicate UPS status.
Reserve
Battery time remaining to end of discharge
RFI
Radio Frequency Interference
RM
Rectifier Magazine
Root Mean Square (RMS)
A modified average. Averaging a sine wave would give a zero, so to obtain meaningful values, the wave is first squared (S), then averaged over one period (M) and finally the square root taken (R). In a sine wave, the factor between RMS and peak is the square root of two.
RS-232
The standard for serial interfaces (serial refers to the eight bits of each character successively sent down one wire) used by most computers, modems and printers.
RS-232C
A common point-to-point hardware configuration for serial
communications.
RS-485
A multidrop hardware configuration for serial communications.
There is no intrinsic method of bus collision detection in RS-485,
so higher layers in the protocol stack must take this into
account.

Scalable UPS
A UPS that allows for expandability; for example, enables a UPS to
accommodate a larger load by purchasing additional power modules.
Simple Network Management Protocol (SNMP)
A User Datagram Protocol (UDP)-based
network protocol. It’s used mostly in
network management systems to
monitor network-attached devices for
conditions that warrant administrative
attention.
Sine Wave
A mathematical function that plots three
qualities of an electrical signal over time:
amplitude, frequency and phase. Clean,
uninterrupted power is represented by a
sine waves, which can also resemble
ocean waves, though they're rarely
perfect.
Single Phase (1Ø) –
Read more here
Power system with one primary waveform. Lower-capacity distribution of power using only one portion of a power source that’s three-phase, like what's supplied by most electric utilities. Used for heating and lighting, no large motors or other heavy-drain devices.

Sliding Demand
Calculating average demand by averaging
demand over several successive time
intervals, advancing one interval at a time.
Slope Discrimination Method
A scheme that causes the Overvoltage Shutdown set point to fall
with increasing load.
SNMP
Simple Network Management Protocol
Split-phase UPS
A UPS with two output phases
referenced to a neutral connection with a
specific phase displacement between
phases, which allows flexibility in load
configuration while maintaining the
availability of bypass. A split-phase UPS
can provide 120V and 208V on the output
simultaneously without the use of an
external transformer. The capabilities for
output are:
- Phase to neutral 100, 110, 120 or 127 Vac
- Phase to phase 200, 208, 220, 230, 240 Vac
Square Wave
Output waveform generated by very basic, low-cost UPSs. Functions
adequately for less sensitive loads, but may not provide
acceptable quality input for some types of electronic equipment.
Standby
UPS type that "stands by," waiting for a power problem from the utility company and rapidly switching to UPS battery power to protect equipment against power failures, sags and surges.
Start-On-Battery
Enables user to power up UPS in the absence of utility power.
Start Up Delay
The interval between power on and the start of current walk in. It
is the sum of the Primary Enable Delay and the fixed and
adjustable portions of the Output Enable Delay.
Static Switch
An electrical component in a UPS that
turns power flow on and off on command
without moving or mechanical
components.
Status LEDs
Light Emitting Diodes (LEDs) that show the status of the UPS when
they light up or turn off.
Step Load
An instantaneous change in the loading
conditions presented to the output of
a UPS
Step Wave
(Modified Sine wave) Enhanced version of square wave that provides
adequate input for some more sensitive loads, but still not as
high quality as a sine wave.
Supervisory Module
The module that monitors and controls the operation of the DC
power system.
Surge
A transient (or momentary) wave of current, potential, or power in
an electric circuit.
Switching Frequency
The rate at which the source voltage
is switched in a switching regulator
or chopped in a DC-to-DC converter.
System Voltage
The nominal voltage of the power system, equal to the
nominal voltage of the rectifier modules. 48 V or 24 V.

Technischer Uberwachungs-Verein (TUV)
An independent non-profit organization that tests and certifies electrical equipment for public safety in the U.S. and worldwide.
Temperature Compensation
Adjustment of the rectifier output voltage to provide the optimum
charging voltage for the battery. One of the components in system
voltage control, calculated by the Supervisory Module calculation
based on battery temperature.
Temperature Sensor
A sensor that is used to produce a variable electrical output
representing the temperature of a component, typically a battery.
Terminal Block
An insulating base equipped with terminals for connecting
secondary and control wiring. Used on hardwired equipment, such as
a UPS, when input plugs and output receptacles are either
impractical or unavailable.
Terminal
A connector for attaching a conductor to an electrical apparatus.
Thermal Regulation
Monitoring the temperature of the
batteries to ensure proper charging.
Three Phase (3Ø) –
Read more here
Power supplied through at least three wires, each carrying power from a common generator but offset in its cycle from the other two. Used for heavy-duty applications.

Topology (UPS)
The core technology of a UPS. Typically, a
UPS is either standby, line interactive or
online though other hybrid technologies
have been introduced.
Total Harmonic Distortion (THD)
How much the circuit voltage deviates
from a perfect sine wave. When viewed
on a meter, a poor voltage THD is most
often manifested in a flat-topped
waveform that comes from the inability of
a power source to respond to the
demands of highly nonlinear loads.
Transfer Switch
A switch which will transfer current from one circuit path to
another without interrupting the flow of the current.
Transfer Time
The length of time it takes a UPS to
transfer to battery power. Typically
measured in milliseconds (ms).
Transformer (T)
A magnetic device that converts AC voltages to AC voltages at any level. An ideal transformer is a lossless device in which no energy is stored that requires no magnetic current.
Transient
A temporary and brief change in a given parameter, typically associated with input voltage or output loading parameters.
Trickle Charge
With the trickle charging process, the battery receives a constant
voltage feeding a low current. Constant use of this method dries
the electrolyte and corrodes the plate, reducing potential battery
service life by up to 50 percent.
Two-Phase Power
Power which is provided by a single source with two outputs which
may be 180 degrees out of phase or 120 degrees out of phase.

Unbalanced Load
An AC power system using more than two wires, where the current is not equal due to an uneven loading of the phases.
Underwriters Laboratories (UL)
An independent non-profit organization
that tests for public safety in the U.S. UL
recognition is required for equipment
used in some applications.
Uninterruptible Power System (UPS)
(1) An electrical system designed to
provide instant, transient-free backup
power during power failure or fault. Some
UPSs also filter and/or regulate utility
power (line conditioning).
(2) A Device
whose sole purpose is to save your
equipment, your data and your job.
UPS Topology
Overall term describing the internal circuitry of a UPS. There are
three basic UPS topologies: standby (off-line), line-interactive,
and online.
User Replaceable
Capable of being replaced by an end user.
Connected equipment may need to be
shut down first. Also see “hot
swappable.”
User-Replaceable Batteries
User replaceable batteries allow the user to easily exchange UPS
batteries, once the unit has been turned off.

Variable Module Management System
(VMMS)
Innovative technology from Eaton that
maximizes UPS efficiencies at low load
levels while supplying the load with
continuous double-conversion power.
Virtualization
The creation of a virtual (rather than
actual) version of something, such as an
operating system, server, storage device
or network resource. Operating system
virtualization is the use of software to
allow a piece of hardware to run multiple
operating system images at the same
time.
Volt/Voltage (V)
Electrical pressure that pushes current
through a circuit. High voltage in a
computer circuit is represented by 1,
while low (or zero) voltage is represented
by 0.
Volt Amps (VA)
The voltage applied to a given piece of equipment, multiplied by the current it draws. Not to be confused with watts, which are similar but represent the actual power drawn by the equipment, and can be somewhat lower than the VA rating.

Walk-In-Time
The time that the rectifier takes to reach rated output current
after the Start Up Delay. The slope is fixed so that a lower
output current will have a shorter walk in period.
Walk-In
The process of gradually ramping up rectifier output voltage (and
current) at start up to prevent a large input current surge.
Watts (W)
The measure of real power. It’s the rate of
doing electrical work. W x 1.3 = VA.
Wye Connection
A connection of three components made
in such a manner that one end of each
component is connected. It’s generally
used to connect devices to a three-phase
power system.
Product List

- PC, Workstation & Home AV UPS
- Eaton 3S (350-750 VA)
- Eaton 5S (550 - 1500VA)
- Network, Server & Storage
- Eaton 5 Series
- Eaton 5SC (500 - 1500VA)
- Eaton 5P (750-3000 VA)
- Eaton 5P Rack (550-3000 VA)
- Eaton 5PX (1000-3000 VA)
- Eaton 9130 (700-3000 VA)
- Eaton 9SX (700-6000 VA)
- Eaton 9PXM (4-20 kVA)
- Eaton 9PX (700VA-11 kVA)
- Eaton 9155 (8-15 kVA)
- Eaton RACKPACKIT (6 kVA)
- Data Center & Facility UPS
- BladeUPS (5-60 kW)
- Eaton 9355 (10 - 30 kVA)
- Eaton Emergency Lighting UPSs - (8-200 kVA)
- Eaton 93E (20 - 60 kVA)
- Eaton 93PM (10-400 kW)
- Eaton 9390 (20-160 kVA)
- Eaton 9390IT (40 kVA)
- Power Xpert 9395 (200-1200 kVA)
- Industrial & Marine UPS
- Eaton FERRUPS (500 VA-18 kVA)
- Eaton FERRUPS RM 60Hz (1.4-7.0 kVA)
- Eaton 9155 Marine (8-30 kVA)
- Eaton 9355 Marine (8-40 kVA)
- Eaton 9PHD Marine (30-200 kVA)
- Power Xpert 9395 Marine (225-1100 kVA)
- Power Distribution
- Rack-mounted Power Distribution
- Floor-based Power Distribution
- Surge Suppression
- Services
- UPS Services
- Batteries
- Remote Monitoring
- Power Management
- Software
- Intelligent Power Manager (IPM)
- Intelligent Power Protector (IPP)
- Connectivity
- Encls, Racks, Cages & Airflow Mgmt
- Airflow Management & Cooling Solutions
- Racks, Enclosures & Cages
- RS Enclosure
- Power Conditioning
- DC Power
- Technical & Office Furniture
- Command Consoles
- Office Furniture
- Lab Furniture
- Legacy Products