Green By Design
Eaton is constantly working with customers to develop solutions that drive sustainable growth around the globe. Our UPS solutions strive for unparalleled energy-efficiency, the efficient use of resource, the maximised use of recyclable materials and the reduction of emissions throughout the entire life of the product, from cradle to grave.
Find out more below about the four steps in Eaton's 'Green by design' product life cycle, from design and manufacturing through to use and end of life.
Use the Energy Calculator
and learn how Eaton UPS's perform with your load profile.
Calculate your total cost of ownership with
Eaton's TCO Calculator.
Life Cycle Assessment (LCA)
Taking account of the environment is a part of the design process at Eaton. Four characteristics guide the design team during their work: energy efficiency, resource efficiency, recycling and compliance with regulations. The Life Cycle Assessment (LCA) process is used to gather information about the potential environmental impact of a product. This process takes place on selected products and assessments adhere to the ISO 14040/14044 standards."LCA results for Eaton 9395 UPS show that 74% of the impacts stem from energy losses in the UPS and 25 % from cooling energy." For more information please contact LCA@eaton.com
Substances and Materials
RoHS Directive (2011/65/EU): Restriction of the Use of Certain Hazardous Substances in Electrical and Electronic Equipment
The Directive applies to electrical and electronic products and restricts the use of some substances, such as heavy metals and certain flame retardants in homogenous materials. Eaton has a proactive approach to environmental legislation and as such is seeking to comply with the RoHS Directive in advance of it becoming a legal requirement to do so. To find RoHS certification for specific products, please see the list of all the certificates.
REACH Regulation (EC 1907/2006): Registration, Evaluation, Authorisation and restriction of Chemicals
The Regulation applies to all electrical products and aims to reduce the use of hazardous chemicals in manufacturing. Eaton is constantly monitoring the use of substances that fall under the REACH Regulations in its manufacturing processes. Our products do not contain SVHCs (Substances of Very High Concern) and if those substances are ever discovered above the threshold limit we will communicate it to our customers as required.
Download the Eaton REACH commitment letter (pdf)
To gather substances and materials information about our UPS standard IEC 62474 (Material Declaration for Products of and for the Electrotechnical Industry) is used as guideline For more information please contact ProductStewardship@Eaton.com
Eaton Green Leaf
The Eaton Green Leaf label is our promise to customers, consumers and our communities, of exceptional and documented environmental performance.
|
International Committees and Organisations
Eaton demonstrates its commitment to protecting the environment through its involvement in IEC standardisation (International Electrotechnical Commission) committees, regulation research studies and non-profit activities such as the Green Grid organisation and the Energy Star programme.
Managing Environment, Safety and Health
Eaton is focused on building sustainable operations and products through the standardisation, globally, of its Environmental, Health and Safety (EHS) programmes and practices. Our global Managing Environment, Safety and Health (MESH) programme is a unified system that consolidates existing programmes (ISO 14001, OHSAS 18001, OSHA VPP) into a single integrated management system.For more information go to: EHS at Eaton
To view ISO 14001 certificates for our sites and manufacturing plants, visit the Power Quality section on the Certificates site.
Green Technology
Eaton develops solutions that are designed to drive sustainable growth around the globe. Our engineers are constantly developing smarter ways to deliver ecological and economic benefits. This includes the development of energy efficient and environmentally friendly technologies. To see how our technology can help you, why not use the Energy Calculator and learn how Eaton UPS's perform with your load profile. Calculate your total cost of ownership with Eaton's TCO Calculator.Energy Saver System (ESS)
The ESS enables extremely high energy efficiency and reliability under normal operating conditions where the load is fed through a static bypass switch. The UPS itself (the rectifier and inverter) is only engaged when the mains power either fails or deviates from pre-set limits in terms of voltage or frequency. Eaton products offer extremely high energy efficiencies compared to other solutions, with rapid transfer to the inverter in the case of mains power failure, thus ensuring no loss of data or disturbance to output. This makes the system more reliable from the load's side. Products that include this technology are the Eaton 9390, 9395 and 9395P UPSs.Easy Capacity Test (ECT) technology
ECT technology enables the user to test their entire power train under full load stress without the need for an external load, thereby reducing the need for dummy loads on installation sites which can give energy savings by making use of idle power. Products that include this technology are the Eaton 9355, 9390, 9395 and 9395P UPSs.Hot Sync technology
With HotSync technology multiple UPSs can be paralleled for increased power capability. The advantage of HotSync technology is that there is no need to purchase an oversized UPS to cope with potential future demands. It is possible to start from a single module and add power when required. Products that include this technology are the BladeUPS, Eaton 9PX, 9155, 9355, 9390, 9395 and 9395P UPSs.Advanced Battery Management (ABM) technology
ABM increases the life of batteries by employing a three-stage charging technique, thereby reducing waste and materials. By eliminating the need for constant charging ABM also helps to reduce energy consumption and extend battery life. Products that include this technology are the BladeUPS, Eaton 5PX, 9130, 9SX, 9PX, 9155, 9355, 9390, 9395, 9395PUPS.Hot Swappable batteries
This technology allows batteries to be 'hot swapped'; replaced or removed one string at a time while the equipment is still running, which reduces battery waste and minimises downtime. Products that include this technology are the BladeUPS, Eaton 5130, 5PX, EX, 9130, 9SX and 9PX UPSs.EcoControl technology
EcoControl automatically disables peripherals when the master drive is turned off, allowing for up to 30 per cent energy savings. This innovative technology can play a strong role in helping to reduce utility bills. A product that includes this technology is the Eaton Ellipse ECO.End of Life
Eaton's End of Life policy is to design products that have a minimal impact on the environment. We are committed to adhering to the following legislation when applicable:WEEE (Directive 2002/96/CE):
Waste Electrical and Electronic Equipment
Eaton WEEE commitment letter (pdf)
Batteries (Directive 2006/66/CE):
Batteries and accumulators and waste batteries and accumulators
Eaton Batteries commitment letter (pdf)
Packaging (Directive 2004/12/CE):
Packaging and packaging waste
Eaton Packaging commitment letter (pdf)
We take into account the environmental effects of the packaging and the end-of-life processing of our products and to aid more responsible dismantling, end-of-life instructions are available for recyclers.
Up to 90% of lead-acid batteries are recycled and majority of the battery material can be used to make new batteries.