Frequently Asked Questions (FAQ)
Here you will find some frequently asked power-related questions. If your question isn’t answered here, please submit your inquiry.
What’s the difference between a surge protector and a UPS?
How much capacity of a UPS should I use?
How much UPS battery runtime do I need?
How is battery runtime impacted if I reduce the load on the UPS?
My business is too small for protective measures. Do I really need a UPS?
Why is power quality such a problem today?
Are power quality problems always noticeable?
How is reliability measured?
How are phone systems and IT equipment affected by inconsistent power?
We have a generator. Do I still need a UPS?
How much UPS capacity do I need?
What are the different levels of surge protection?
What happens if the UPS is overloaded, for example, if the protected equipment and/or load draws more current than it can provide?
What causes a UPS to be overloaded?
I have a 3000 VA UPS. Can I just plug the unit into a standard 15A wall outlet?
Why is power management software important?
Will my current UPS software monitor my new Eaton UPS?
My data center only went down for a couple of minutes. What’s the big deal?
Where can I get technical help?
For a smaller server rack, what are my options?
Where in the room should I put my rack or enclosure?
How much space should go between racks or enclosures?
What are the least expensive ways to organize cabling and equipment in my racks or enclosures?
Why shouldn’t I run cables horizontally between racks and enclosures?
Questions welcome! We invite you to submit your power related question here.
What’s the difference between a surge protector and a UPS?
A surge protector provides just that—surge protection. In addition to surge protection, a UPS continually regulates incoming voltage and provides battery backup in the event of a power failure. You'll often see surge protectors plugged into a UPS for added surge protection and additional output receptacles.
How much capacity of a UPS should I use?
To allow for future expansion, we recommend that you install a UPS at approximately 75 percent capacity. In addition, the batteries degrade over time; by oversizing, you provide room for error. In the online Eaton UPS sizing tool, we’ve included a “capacity used” column.
How much UPS battery runtime do I need?
During an outage, you need enough battery runtime to gracefully shut down systems or switch to backup generators. You may add an optional external battery module (EBM) to increase runtime. For a UPS battery overview and factors affecting battery life, request a UPS Fundamentals Handbook.
How is battery runtime impacted if I reduce the load on the UPS?
There can be a significant increase in runtime. Generally speaking, a UPS that provides five minutes at full load will provide 15 minutes at half load.
My business is too small for protective measures. Do I really need a UPS?
Power problems are equal-opportunity threats. Your PCs, servers and network are just as critical to your business as a data center is to a large enterprise. Downtime is costly in terms of hardware and potential loss of goodwill, reputation and sales. Also add in the delays that inevitably occur when rebooting locked-up equipment, restoring damaged files and re-running processes that were interrupted. A sound power protection strategy is cost-effective insurance.
Why is power quality such a problem today?
Today’s high-tech IT equipment and control units are much more sensitive to electrical disturbances and are more important to the critical functions of many businesses than in the past. As a result, power quality problems today are more frequent and more costly than ever. Check out the nine power problems here.
Are power quality problems always noticeable?
No. In many cases, disturbances can cause imperceptible damage to circuits and other components, a major cause of premature equipment failure and problems like computer lockups. Many power quality problems go unresolved, resulting in lost revenue and data.
How is reliability measured?
Power reliability is usually stated as a percent of time the power is available. For example, the power grid system in the U.S. provides three nines of reliability—the power is available for 99.9 percent of the time. Because those 8.8 hours of downtime translate into significant downtime and expense, IT and telephone network services require at least five nines of reliability.
How are phone systems and IT equipment affected by inconsistent power?
Fluctuating power is a waste of valuable time and money. If customers expose their telephone systems (and any other electronic equipment) to inconsistent utility power, they’re vulnerable to hardware and software damage, data corruption and communication breakdown. The time and cost of replacing equipment, as well as the business lost during breakdown and replacement, can greatly affect a company’s bottom line.
Reliability average | Non-availability per year |
---|---|
99% | 88 hours |
99.9% | 8.8 hours |
99.99% | 53 minutes |
99.999% | 5.3 minutes |
99.9999% | 32 seconds |
99.99999%+ | 3.2 seconds |
We have a generator. Do I still need a UPS?
A generator will NOT protect your equipment against power problems. You need a UPS to guarantee that the equipment stays up until the generator kicks on and stabilizes—which often requires several minutes.
How much UPS capacity do I need?
Determine the total load (in watts) of the equipment you want to protect. Add 10–20 percent for future growth and decide the minimum amount of runtime you need. Use the online sizing tool to identify the right solution for your application.
What are the different levels of surge protection?
There are three typical levels :
- Lightning arrestors. Big and mean, usually found in large facilities located in high-risk areas. Takes an extremely high voltage and clamps it down.
- Surge Protective Devices (SPD or TVSS). Mounted on your panelboard or load center; sometimes larger UPS models may have some level of this, but typically not a great amount. Clamps voltage down two even lower tolerances (~1 kV or less).
- Local outlet level surge protector. A simple surge strip; small plug-and-play UPSs often have this as well. Brings voltage down to levels that will not permanently damage connected equipment (typically ~380V).
Lightning strikes have such an incredible amount of energy that only an expensive lightning arrestor would protect you from a direct hit and they often don't guarantee complete protection. For the best protection against lightning strikes, you want to develop a two-stage defense with something at your panel and something at the outlet level. Visit the Surge Protection Devices page for some informative videos and additional information.
What happens if the UPS is overloaded, for example, if the protected equipment and/or load draws more current than it can provide.
The UPS transfers the load to bypass (for a few minutes) until the overload condition is reversed. If the overload condition continues, some UPS models automatically shut down. Some models can run at 110V indefinitely in bypass.
What causes a UPS to be overloaded?
There are two possible answers: (1) the UPS was undersized (e.g., the load is rated at 1200 VA, but a 1000 VA UPS was provided), or (2) you plugged more equipment into the UPS than it was designed to handle.
I have a 3000 VA UPS. Can I just plug the unit into a standard 15A wall outlet?
Only UPSs with power ratings up to 1500 VA plug into a standard 15A wall outlet. All others require a larger receptacle, which must be installed by an electrician. View our guide on input plugs and output receptacles.
Why is power management software important?
Although UPSs are typically rugged and reliable, they do require ongoing monitoring and support. Power management software continuously monitors and diagnoses the state of the grid, batteries and power sources, together with the condition of the UPS’s internal electronics. Eaton UPS software and connectivity cards enable remote monitoring and management capability, including graceful shutdown and load segment control.
Will my current UPS software monitor my new Eaton UPS?
Yes, you can monitor your Eaton UPS with any UPS or facility management software that supports the industry standard Management Information Base (MIB, RFC 1628) as long as you install the optional connectivity card. Most UPS vendors support this MIB and all good facility management software, including OpenManage, OpenView and Tivoli also support it. Extended Eaton Advanced MIBs are available for greater levels of detail.
You can remotely control your Eaton UPS using the Eaton UPS management software or through a secure web interface if you choose the optional connectivity card, which also allows for automated email alerts for power events without needing to install any software.
My data center only went down for a couple of minutes. What’s the big deal?
When a data center goes down and then back up during a power outage without a managed shut down, it doesn't come up nicely. Storage arrays initialize after servers that try to mount their shares, while some servers boot without access to DNS servers that are also booting and thus have other problems. Although the outage was short, it can take hours to get everything back online. In addition, data corruption is a serious concern.
Where can I get technical help?
Contact your territory representative or call the Eaton UPS hotline at 1-800-356-5794 for pre-sales support and 1-800-356-5737 for technical support. You can also visit our Contact Us page
For a smaller server rack, what are my options?
Often a 42U enclosure—which is the most common—is not required. Smaller options such as 25U, 30U or 36U will provide more than enough rack mounting space for servers, UPSs, rack PDUs, switches and other equipment. The smaller options enable you to use the space on top for monitors or other equipment. Features such as perforated doors, adjustable rails, locks and casters are still available in these sizes. Wall mount enclosures can also be considered when a full-height rack or enclosure isn’t necessary.
Where in the room should I put my rack or enclosure?
A good rule of thumb is four feet of space, front and back, from the wall. Fire codes require three-foot walkways, but four feet will allow you to wheel a cart in the room safely and reduce human error overall. In the future, if you have equipment to install, you may need two people in the space at a time lifting, and you want enough space to comfortably get the work done. Otherwise, your rack location will be determined by your unique space. It needs to be in a place that has the appropriate electrical requirements and ample space to run corresponding data and power cables.
How much space should go between racks or enclosures?
Ideally, your racks and enclosures should be side by side and can be bolted together. This is often called baying or ganging, and it allows you to maximize floor space and be more efficient while servicing the equipment stored in them. Remember, space is an invaluable resource in IT!
What are the least expensive ways to organize cabling and equipment in my racks or enclosures?
Velcro straps for data and power cables and labels are the easiest and most affordable way to organize your racks, at a base level, and will likely have the biggest impact from an access and service standpoint.
Why shouldn’t I run cables horizontally between racks and enclosures?
You can run cables horizontally between racks, but you must ensure you’re using the appropriate cable management devices to do so. If you simply run cables directly across—rather than up the side of the rack or enclosure to horizontal cable management devices—it will cause problems for you when you go to change out or service equipment as well as if you need to move a rack or enclosure.
Product List

- PC, Workstation & Home AV UPS
- Eaton 3S (550-750 VA)
- Eaton 5S (550 - 1500VA)
- Network & Server
- Eaton 5SC (500 - 1500VA)
- Eaton 5P (750-3000 VA)
- Eaton 5P Rack (550-3000 VA)
- Eaton 5PX (1000-3000 VA)
- Eaton 9130 (700-3000 VA)
- Eaton 9130 RM (700-3000 VA)
- Eaton 9PX (2-3 kVA)
- Eaton 9PX (5-11 kVA)
- Eaton 9170+ (3-18 kVA)
- Eaton 9155 (8-15 KVA)
- Data Center & Facility UPS
- BladeUPS (12-60 kW)
- Eaton 9355 (10-40 kVA)
- Eaton 93E (20 - 60 kVA)
- Eaton 93PM (50-100 kW)
- Eaton 9390 (40-160 kVA)
- Eaton 9390IT (40 kVA)
- Power Xpert 9395 (225-1100 kVA)